Question
Can you confirm that the ADF4113HV only has two charge pump current settings
compared to the ADF4113's 8 different settings (refer to page 17 of datasheet
Rev. D)?
Answer
Firstly, the ADF4113HV and ADF4113 may have similar names, but they are built
on two different technologies.
Yes, the ADF4113HV only has the two charge pump current settings. The charge
pump current can be adjusted via Rset.
The major difference between these devices is charge pump supply. The maximum
charge pump supply for the ADF4113 is 6V and for the ADF4113HV is 16.5V