The Warning 61=0x3D is just for information (like most warnings) and it is recommended to clear the warning after being read.
This warning code 61 is issued whenever one or more of the CORR DC offset DACs either saturate or the algorithm cannot converge within a certain number of iterations. This could occur when the power level is changing. Note that the firmware will automatically address this and no action is required, except clearing the warning message.
This warning code 61 is issued whenever one or more of the CORR DC offset DACs either saturate or the algorithm cannot converge within a certain number of iterations. This could occur when the power level is changing. Note that the firmware will automatically address this and no action is required, except clearing the warning message.