AD831: FAQ
AD8315
Production
The AD8315 is a complete low cost subsystem for the precise
control of RF power amplifiers operating in the frequency range
0.1 GHz to 2.5 GHz and over...
Datasheet
AD8315 on Analog.com
AD8317
Production
The AD8317 is a demodulating logarithmic amplifier, capable of accurately converting an RF input signal to a corresponding decibel-scaled output. It employs...
Datasheet
AD8317 on Analog.com
AD8319
Recommended for New Designs
The AD8319 is a demodulating logarithmic amplifier, capable of accurately converting an RF input signal to a corresponding decibel-scaled output. It employs...
Datasheet
AD8319 on Analog.com
AD8314
Production
The AD8314 is a complete low cost subsystem for the measurement and control of RF signals in the frequency range of 100 MHz to 2.7 GHz, with a typical...
Datasheet
AD8314 on Analog.com
AD8311
Recommended for New Designs
The AD8311 is a complete low cost subsystem for the precise control of RF power amplifiers operating in the frequency range 0.1 GHz to 2.5 GHz and over...
Datasheet
AD8311 on Analog.com
AD8318
Recommended for New Designs
The AD8318 is a demodulating logarithmic amplifier, capable of accurately converting an RF input signal to a corresponding decibel-scaled output voltage...
Datasheet
AD8318 on Analog.com
AD8310
Production
The AD8310 is a complete, dc to 440 MHz demodulating logarithmic amplifier (log amp) with a very fast voltage mode output, capable of driving up to 25...
Datasheet
AD8310 on Analog.com
AD8312
Recommended for New Designs
The AD8312 is a complete, low cost subsystem for the measurement of RF signals in the frequency range of 50 MHz to 3.5 GHz. It has a typical dynamic range...
Datasheet
AD8312 on Analog.com
AD8313
Production
The AD8313 is a complete multistage demodulating logarithmic amplifier that can accurately convert an RF signal at its input to an equivalent decibel-scaled...
Datasheet
AD8313 on Analog.com