Post Go back to editing

custom board, ad9209 init failed at pre clock init stage.

Thread Summary

The user encountered a Pre Clock Boot Sequence Error while configuring the AD9209 ADC with a 250 MHz clock. The issue was resolved by correcting the SVDD2_PLL supply voltage from 1V to 2V, despite the supply monitor registers indicating no issues. The clock input signal was confirmed to be 250 MHz with the correct amplitude and impedance settings.
AI Generated Content
Category: Software
Product Number: AD9209
Software Version: AD9209 API v1.7.0

I am using AD9209 in the following configuration

{ 250e6, 250e6, 6000e6, 2000e6 }, /* uc42, 204B, 250MHz, 10Gbps, 8L-8M-1S-16NP, 2GSPS/4x dcm */

I am getting a Pre Clock Boot Sequence Error.

With the oscilloscope, I can see the 250MHz for the ADC on my custom board.

I am not able to find any description for the 0x3740 to 0x3743 registers.

LOG: 

Hello World
ads9_hw_open: SPI (AD9209@0x44A70000, HMC7044@0x44A00000) GPIO ch2: rstb=1 rxen=1 hmc_sync=0
Found connected device board: AD9209-FMCA-EBZ RevA
On board crystal select: 100000000Hz
adi_ad9209_device_api_revision_get(...)
AD9209 API v1.7.0
FPGA Image v0 sv0
APP: Configure Usecase:42, Tx Path: DAC Clk: 6000000000, JESD Rx Mode: 0 & Rx Path: ADC CLK: 20000000
adi_ad9209_device_reset(...)
APP: Tx Lane Rate : 0 Rx0 Lane Rate: 10000000000 Rx1 Lane Rate : 0
APP: Configure Platform Reference Clocks
APP: Reference Clocks Configured
APP: Configure FPGA JESD Interfaces
APP: FPGA JESD Interfaces Configured
APP: Configure ad9209 Device
adi_ad9209_device_reset(...)
ad9209: w@0000 = 81
ad9209: w@0000 = 00
adi_ad9209_device_init(...)
api v1.7.0 commit 5fc9176 for ad9209
host is using little endian mode.
adi_ad9209_device_spi_config(...)
ad9209: w@0000 = 3c
adi_ad9209_device_reg8_access_check(...)
ad9209: r@801c = ff
ad9209: w@001c = 5a
ad9209: r@801c = 5a
ad9209: w@001c = a5
ad9209: r@801c = a5
ad9209: w@001c = ff
adi_ad9209_device_power_status_check(...)
ad9209: r@8210 = 3f
ad9209: r@8211 = 0f
ad9209: r@8212 = 3f
ad9209: r@8213 = 3f
adi_ad9209_device_clk_config_set(...)
adi_ad9209_device_boot_pre_clock(...)
ad9209: r@b742 = 33 (100 TIMES)
Pre Clock Boot Sequence Error
Please check power supplies (no open, no short, no big glitches)
Ensure Clocks are available
ad9209: r@b740 = 02
ad9209: r@b741 = 60
ad9209: r@b742 = 33
ad9209: r@b743 = 00
adi_ad9209_device_clk_pll_lock_status_get(...)
ad9209: w@00d0 = 0a
ad9209: r@80d0 = 0a
ad9209: w@00ec = 22
ad9209: r@80ec = 26
ad9209: r@a008 = 02
APP: Clock Configuration error

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.