Post Go back to editing

AD9986 valid interpolator settings

Thread Summary

The user inquired about the differences in interpolation values for AD9986 Mode 18 between JESD204B and JESD204C. The support engineer explained that the differences are due to changes in link parameters (F, S, K, and E) between the two standards, which affect the valid interpolation modes. The user also asked about Mode 16.00 decimation configurations, specifically why a total decimation of 12 allows coarse 6, fine 2 but not coarse 4, fine 3. The engineer indicated that this is an architectural limitation, not a validation issue.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD9986

For the AD9986 table 92 in UG-1578 indicates that mode 18 allows for 8 lanes for two converters running with a wide variety of coarse interpolation values (1,2,4,6,8x1) in JESD204B mode.  However table 93 indicates that mode 18 in JESD204C mode only runs with interpolation values of .  1x1, 2x1, 2x2, and 4x1.  Is this a documentation issue?  An actual hardware limitation?  A matter of some modes not being validated by ADI?  Why the difference between 204B and 204C?

Parents
  • Following up again - it looks like mode 32.00 supports both 4x3 and 6x2 decimation for total decimation of 12, but that mode transfers 24 bits per sample across the JESD link, requiring 50% faster clock speeds.  Is it really the case that the equivalent 16.00 mode only supports 6x2 decimation, and not 4x3?
    Highlighting the two modes below for reference:

    We're running up at 6 gsps.  It seems like the data path (CDDC, FDDC) can handle the data rates with 4x3 decimation based on the mode 32 options, and it's not clear why the JESD layer would how the decimation was split between fine and coarse as long as the total decimation equals 12.  For our application we'd much rather not move to mode 32 which stresses the JESD lanes more, and draws more power, so any feedback on the plausibility of the highlighted mode 16 supporting 4x3 decimation would be much appreciated.

    Thanks!

Reply
  • Following up again - it looks like mode 32.00 supports both 4x3 and 6x2 decimation for total decimation of 12, but that mode transfers 24 bits per sample across the JESD link, requiring 50% faster clock speeds.  Is it really the case that the equivalent 16.00 mode only supports 6x2 decimation, and not 4x3?
    Highlighting the two modes below for reference:

    We're running up at 6 gsps.  It seems like the data path (CDDC, FDDC) can handle the data rates with 4x3 decimation based on the mode 32 options, and it's not clear why the JESD layer would how the decimation was split between fine and coarse as long as the total decimation equals 12.  For our application we'd much rather not move to mode 32 which stresses the JESD lanes more, and draws more power, so any feedback on the plausibility of the highlighted mode 16 supporting 4x3 decimation would be much appreciated.

    Thanks!

Children
No Data