Post Go back to editing

Input Clock Configuration

Thread Summary

The user asked if the central clock pins (P1/R1) need to be connected to a clock source when using the A & B side clock pins (CLKA and CLKB) with complementary SYSREFs. The final answer confirms that the central clock pins can be left floating if the A & B side clock pins are used.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD9084

I'm seeking clarification on the following, we plan to connect a clock source to CLKA (Pins AF3/AG3) and CLKB (Pins C3/D3) for Bank A and B respectively (complimentary SYSREFs have also been connected).

The question  - do the CLK (Pins P1/R1) also need to be connected to a clock source or can these pins be left floating? 

Parents Reply Children
No Data