Post Go back to editing

Input Clock Configuration

Thread Summary

The user asked if the central clock pins (P1/R1) need to be connected to a clock source when using the A & B side clock pins (CLKA and CLKB) with complementary SYSREFs. The final answer confirms that the central clock pins can be left floating if the A & B side clock pins are used.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD9084

I'm seeking clarification on the following, we plan to connect a clock source to CLKA (Pins AF3/AG3) and CLKB (Pins C3/D3) for Bank A and B respectively (complimentary SYSREFs have also been connected).

The question  - do the CLK (Pins P1/R1) also need to be connected to a clock source or can these pins be left floating? 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.