Post Go back to editing

Unused JESD Pins

Thread Summary

The user inquired about using the AD9084 with a JESD controller that supports 32 lanes (16Rx/16Tx). The AD9084 supports up to 24 lanes (12Tx/12Rx per side) and can be configured as single or dual links. Unused pins should be powered down by firmware and can be left floating.
AI Generated Content
Category: Hardware
Product Number: AD9084

I'm currently working on an AFE hardware design using the AD9084, the JESD controller being used can provide 32 lanes (16Rx/16Tx). Can the AD9084 support this? If so, are there specific pins that should be used and any care to be taken to unused pins?

Thanks.