Post Go back to editing

No output from AD9082 DAC

Thread Summary

The user was unable to get any output on the DAC when using AD9082 with VPK180, despite JESD204 status appearing fine. The issue was resolved by correcting incorrectly wired pins, allowing the design to run successfully at a 12.375 GHz lane rate. The user is now investigating unexpected noise and spikes in the DAC output.
AI Generated Content
Category: Hardware
Product Number: AD9082

Hello, I'm working with AD9082 + VPK180 and can't get any output on the DAC.

JESD status looks fine:

I was able to confirm the ADC path with a signal generator and saw the signal on ADI IIO Oscilloscope.

My JESD Parameters are the following:

					adi,subclass = <1>;			/* JESD SUBCLASS 0,1,2 */
					adi,version = <2>;			/* JESD VERSION 0=204A,1=204B,2=204C */
					adi,dual-link = <0>;			/* JESD Dual Link Mode */
					adi,converters-per-device = <4>;	/* JESD M */
					adi,octets-per-frame = <1>;		/* JESD F */
					adi,frames-per-multiframe = <256>;	/* JESD K */
					adi,converter-resolution = <16>;	/* JESD N */
					adi,bits-per-sample = <16>;		/* JESD NP' */
					adi,control-bits-per-sample = <0>;	/* JESD CS */
					adi,lanes-per-device = <8>;		/* JESD L */
					adi,samples-per-converter-per-frame = <1>; /* JESD S */
					adi,high-density = <1>;			/* JESD HD */

I was able to see an output with the Global TX compartment, applying NCO and generating Test tones, but when trying to use the DDS or transmit from the DMA (both with IIO Oscilloscope) I get absolutely nothing. using Vivado Chipscope, I was able to see that the link interface going out from the tpl_core block has the waveform data and both valid and ready are high, but the output still won't be seen.

Would appreciate any help on the matter, Thank you!

  • Hi, could you confirm that JESD link status on DAC path is also on "Data"?

    -YH

  • Hey, thanks for replying!

    Yes, both rx and tx are on DATA, sorry for not mentioning it in the post:

    Obviously, I noticed the alignment error which I don't recall being there before, but solving that might be the solution overall. I stumbled upon this thread:

     Versal AD9082 FMCA-EBZ M4 L8 JESD204C design - cont. (SYSREF alignment error) 

    Which described the same issue on a VPK120 board, which I also own and tried to use with AD9082 to no success. I went back to the VCK180 because of that but using the VPK120 is actually more beneficial for me.

    I'm pretty lost with that issue so let me know if there is any more info I can provide that will help

    Thank you!

  • Hey, thank you for information. I think my design had some timing violations caused by Xilinx Logic Analyzers. I was to able to fix the issue and now jesd_status is proper:

    But I still see no output from the DAC, same as before. In the ILAs the Link interface looks fine and JESD signals also look fine so I'm not sure how to tackle this issue next. I would gladly take any advice, thank you!

  • I will attach some more relevant info:
    my device tree:

    #include <dt-bindings/gpio/gpio.h>
    #include <dt-bindings/iio/frequency/hmc7044.h>
    #include <dt-bindings/iio/adc/adi,ad9081.h>
    #include <dt-bindings/interrupt-controller/irq.h>
    #include <dt-bindings/jesd204/adxcvr.h>
    
    /include/ "system-conf.dtsi"
    
    /* RX path */
    #define AD9081_RX_LANERATE_KHZ	24750000
    #define AD9081_RX_LINK_CLK	375000000
    
    /* TX path */
    #define AD9081_TX_LANERATE_KHZ	24750000
    #define AD9081_TX_LINK_CLK	375000000
    
    / {
    	model = "Analog Devices AD9081-FMC-EBZ-VPK180 Rev.A";
    
    	chosen {
    		bootargs = "console=ttyAMA0 earlycon=pl011,mmio32,0xFF000000,115200n8 clk_ignore_unused root=/dev/mmcblk0p2 rw rootfstype=ext4 rootwait";
    		stdout-path = "serial0:115200";
    	};
    
    	fpga_axi: fpga-axi@0 {
    		interrupt-parent = <&gic>;
    		compatible = "simple-bus";
    		#address-cells = <0x1>;
    		#size-cells = <0x1>;
    		ranges = <0 0 0 0xffffffff>;
    
    		clocks {
    			rx_fixed_linerate: clock@0 {
    				#clock-cells = <0>;
    				compatible = "fixed-clock";
    				clock-frequency = <AD9081_RX_LANERATE_KHZ>;
    				clock-output-names = "rx_lane_clk";
    			};
    
    			tx_fixed_linerate: clock@1 {
    				#clock-cells = <0>;
    				compatible = "fixed-clock";
    				clock-frequency = <AD9081_TX_LANERATE_KHZ>;
    				clock-output-names = "tx_lane_clk";
    			};
    
    			rx_fixed_link_clk: clock@2 {
    				#clock-cells = <0>;
    				compatible = "fixed-clock";
    				clock-frequency = <AD9081_RX_LINK_CLK>;
    				clock-output-names = "rx_link_clk";
    			};
    
    			tx_fixed_link_clk: clock@3 {
    				#clock-cells = <0>;
    				compatible = "fixed-clock";
    				clock-frequency = <AD9081_TX_LINK_CLK>;
    				clock-output-names = "tx_link_clk";
    			};
    		};
    
    		axi_gpio: gpio@a4000000 {
    			#gpio-cells = <2>;
    			#interrupt-cells = <2>;
    			clock-names = "s_axi_aclk";
    			clocks = <&versal_clk PMC_PL0_REF>;
    			compatible = "xlnx,axi-gpio-2.0", "xlnx,xps-gpio-1.00.a";
    			gpio-controller;
    			interrupt-controller;
    			interrupt-names = "ip2intc_irpt";
    			interrupt-parent = <&gic>;
    			interrupts = <0 84 4>;
    			reg = <0xa4000000 0x1000>;
    			xlnx,all-inputs = <0x0>;
    			xlnx,all-inputs-2 = <0x0>;
    			xlnx,all-outputs = <0x0>;
    			xlnx,all-outputs-2 = <0x0>;
    			xlnx,dout-default = <0x00000000>;
    			xlnx,dout-default-2 = <0x00000000>;
    			xlnx,gpio-width = <0x20>;
    			xlnx,gpio2-width = <0x20>;
    			xlnx,interrupt-present = <0x1>;
    			xlnx,is-dual = <0x1>;
    			xlnx,tri-default = <0xFFFFFFFF>;
    			xlnx,tri-default-2 = <0xFFFFFFFF>;
    		};
    
    		rx_dma: dma@bc420000 {
    			compatible = "adi,axi-dmac-1.00.a";
    			reg = <0xbc420000 0x10000>;
    			#dma-cells = <1>;
    			#clock-cells = <0>;
    			interrupts = <0 97 IRQ_TYPE_LEVEL_HIGH>;
    			clocks = <&versal_clk PMC_PL1_REF>;
    		};
    
    		tx_dma: dma@bc430000  {
    			compatible = "adi,axi-dmac-1.00.a";
    			reg = <0xbc430000 0x10000>;
    			#dma-cells = <1>;
    			#clock-cells = <0>;
    			interrupts = <0 96 IRQ_TYPE_LEVEL_HIGH>;
    			clocks = <&versal_clk PMC_PL1_REF>;
    		};
    
    		axi_ad9081_core_rx: axi-ad9081-rx-hpc@a4a10000 {
    			compatible = "adi,axi-ad9081-rx-1.0";
    			reg = <0xa4a10000 0x8000>;
    			dmas = <&rx_dma 0>;
    			dma-names = "rx";
    			spibus-connected = <&trx0_ad9081>;
    
    			jesd204-device;
    			#jesd204-cells = <2>;
    			jesd204-inputs = <&axi_ad9081_rx_jesd 0 FRAMER_LINK0_RX>;
    		};
    
    		axi_ad9081_core_tx: axi-ad9081-tx-hpc@a4b10000 {
    			compatible = "adi,axi-ad9081-tx-1.0";
    			reg = <0xa4b10000 0x4000>;
    			dmas = <&tx_dma 0>;
    			dma-names = "tx";
    			clocks = <&trx0_ad9081 1>;
    			clock-names = "sampl_clk";
    			spibus-connected = <&trx0_ad9081>;
    
    			jesd204-device;
    			#jesd204-cells = <2>;
    			jesd204-inputs = <&axi_ad9081_tx_jesd 0 DEFRAMER_LINK0_TX>;
    		};
    
    		axi_ad9081_rx_jesd: axi-jesd204-rx@a4a90000 {
    			compatible = "adi,axi-jesd204-rx-1.0";
    			reg = <0xa4a90000 0x1000>;
    
    			interrupts = <0 95 IRQ_TYPE_LEVEL_HIGH>;
    
    			clocks = <&versal_clk PMC_PL0_REF>, <&hmc7044 10>, <&rx_fixed_link_clk>, <&rx_fixed_linerate>;
    			clock-names = "s_axi_aclk", "device_clk", "link_clk", "lane_clk";
    
    			#clock-cells = <0>;
    			clock-output-names = "jesd_rx_lane_clk";
    
    			jesd204-device;
    			#jesd204-cells = <2>;
    			jesd204-inputs = <&hmc7044 0 FRAMER_LINK0_RX>;
    
    			reset-done-gpios = <&axi_gpio 32 0>;
    			pll-datapath-reset-gpios = <&axi_gpio 36 0>;
    			datapath-reset-gpios = <&axi_gpio 38 0>;
    		};
    
    		axi_ad9081_tx_jesd: axi-jesd204-tx@a4b90000 {
    			compatible = "adi,axi-jesd204-tx-1.0";
    			reg = <0xa4b90000 0x1000>;
    
    			interrupts = <0 94 IRQ_TYPE_LEVEL_HIGH>;
    
    			clocks = <&versal_clk PMC_PL0_REF>, <&hmc7044 6>, <&tx_fixed_link_clk>, <&tx_fixed_linerate>;
    			clock-names = "s_axi_aclk", "device_clk", "link_clk", "lane_clk";
    
    			#clock-cells = <0>;
    			clock-output-names = "jesd_tx_lane_clk";
    
    			jesd204-device;
    			#jesd204-cells = <2>;
    			jesd204-inputs = <&hmc7044 0 DEFRAMER_LINK0_TX>;
    
    			reset-done-gpios = <&axi_gpio 33 0>;
    			pll-datapath-reset-gpios = <&axi_gpio 37 0>;
    			datapath-reset-gpios = <&axi_gpio 39 0>;
    		};
    
    		axi_sysid_0: axi-sysid-0@a5000000 {
    			compatible = "adi,axi-sysid-1.00.a";
    			reg = <0xa5000000 0x10000>;
    		};
    	};
    };
    
    &gic {
    	num_cpus = <2>;
    	num_interrupts = <96>;
    };
    
    &lpd_dma_chan0 {
    	status = "okay";
    };
    
    &lpd_dma_chan1 {
    	status = "okay";
    };
    
    &lpd_dma_chan2 {
    	status = "okay";
    };
    
    &lpd_dma_chan3 {
    	status = "okay";
    };
    
    &lpd_dma_chan4 {
    	status = "okay";
    };
    
    &lpd_dma_chan5 {
    	status = "okay";
    };
    
    &lpd_dma_chan6 {
    	status = "okay";
    };
    
    &lpd_dma_chan7 {
    	status = "okay";
    };
    
    &cci {
    	status = "okay";
    };
    
    &smmu {
    	status = "okay";
    };
    
    &i2c1 {
    	status = "disabled";
    };
    
    &gpio1 {
    	status = "okay";
    };
    
    &qspi {
    	is-dual = <1>;
    	num-cs = <1>;
    	spi-rx-bus-width = <4>;
    	spi-tx-bus-width = <4>;
    	status = "okay";
    };
    
    &sdhci1 {
    	clock-frequency = <199999985>;
    	status = "okay";
    };
    
    &serial0 {
    	cts-override ;
    	device_type = "serial";
    	port-number = <0>;
    };
    
    &spi0 {
    	is-decoded-cs = <0>;
    	num-cs = <3>;
    	status = "okay";
    };
    
    &spi1 {
    	is-decoded-cs = <0>;
    	num-cs = <3>;
    	status = "okay";
    };
    
    &ttc0 {
    	status = "okay";
    };
    
    &ref_clk {
    	clock-frequency = <33333333>;
    };
    
    &gem0 {
    	local-mac-address = [00 0a 35 ad 90 81];
    };
    
    &fpga_axi {
    	axi_data_offload_tx: axi-data-offload-0@bc440000 {
    		compatible = "adi,axi-data-offload-1.0.a";
    		reg = <0xbc440000 0x10000>;
    	};
    
    	axi_data_offload_rx: axi-data-offload-1@bc450000 {
    		compatible = "adi,axi-data-offload-1.0.a";
    		reg = <0xbc450000 0x10000>;
    	};
    };
    
    &axi_ad9081_core_tx {
    	adi,axi-data-offload-connected = <&axi_data_offload_tx>;
    	adi,axi-pl-fifo-enable;
    };
    
    #define fmc_spi spi0
    
    &spi1 {
    	status = "okay";
    
    	hmc7044: hmc7044@0 {
    		#address-cells = <1>;
    		#size-cells = <0>;
    		#clock-cells = <1>;
    		compatible = "adi,hmc7044";
    		reg = <0>;
    		spi-max-frequency = <1000000>;
    
    		jesd204-device;
    		#jesd204-cells = <2>;
    		jesd204-sysref-provider;
    
    		adi,jesd204-max-sysref-frequency-hz = <2000000>; /* 2 MHz */
    
    		/*
    		 * There are different versions of the AD9081-FMCA-EBZ & AD9082-FMCA-EBZ
    		 * VCXO = 122.880 MHz, XO = 122.880MHz (AD9081-FMC-EBZ & AD9082-FMC-EBZ)
    		 * VCXO = 100.000 MHz, XO = 100.000MHz (AD9081-FMC-EBZ-A2 & AD9082-FMC-EBZ-A2)
    		 * To determine which board is which, read the freqency printed on the VCXO
    		 * or use the fru-dump utility:
    		 * #fru-dump -b /sys/bus/i2c/devices/15-0050/eeprom
    		 */
    
    		//adi,pll1-clkin-frequencies = <122880000 30720000 0 0>;
    		//adi,vcxo-frequency = <122880000>;
    
    		adi,pll1-clkin-frequencies = <100000000 10000000 0 0>;
    		adi,pll1-ref-prio-ctrl = <0xE1>; /* prefer CLKIN1 -> CLKIN0 -> CLKIN2 -> CLKIN3 */
    		adi,pll1-ref-autorevert-enable;
    		adi,vcxo-frequency = <100000000>;
    
    		adi,pll1-loop-bandwidth-hz = <200>;
    		adi,pll1-charge-pump-current-ua = <720>;
    		adi,pfd1-maximum-limit-frequency-hz = <1000000>; /* 1 MHz */
    
    		adi,pll2-output-frequency = <3000000000>;
    
    		adi,sysref-timer-divider = <1024>;
    		adi,pulse-generator-mode = <0>;
    
    		adi,clkin0-buffer-mode  = <0x07>;
    		adi,clkin1-buffer-mode  = <0x07>;
    		adi,oscin-buffer-mode = <0x15>;
    
    		adi,gpi-controls = <0x00 0x00 0x00 0x00>;
    		adi,gpo-controls = <0x37 0x33 0x00 0x00>;
    
    		clock-output-names =
    		"hmc7044_out0", "hmc7044_out1", "hmc7044_out2",
    		"hmc7044_out3", "hmc7044_out4", "hmc7044_out5",
    		"hmc7044_out6", "hmc7044_out7", "hmc7044_out8",
    		"hmc7044_out9", "hmc7044_out10", "hmc7044_out11",
    		"hmc7044_out12", "hmc7044_out13";
    
    		hmc7044_c0: channel@0 {
    			reg = <0>;
    			adi,extended-name = "CORE_CLK_RX";
    			adi,divider = <8>;	// 375
    			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS
    
    		};
    
    		hmc7044_c2: channel@2 {
    			reg = <2>;
    			adi,extended-name = "DEV_REFCLK";
    			adi,divider = <8>;	// 375
    			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS
    		};
    
    		hmc7044_c3: channel@3 {
    			reg = <3>;
    			adi,extended-name = "DEV_SYSREF";
    			adi,divider = <768>;	// 3.90625
    			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS
    			adi,jesd204-sysref-chan;
    		};
    
    		hmc7044_c6: channel@6 {
    			reg = <6>;
    			adi,extended-name = "CORE_CLK_TX";
    			adi,divider = <8>;	// 375
    			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS
    		};
    
    		hmc7044_c8: channel@8 {
    			reg = <8>;
    			adi,extended-name = "FPGA_REFCLK1";
    			adi,divider = <8>;	// 375
    			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS
    		};
    
    		hmc7044_c10: channel@10 {
    			reg = <10>;
    			adi,extended-name = "CORE_CLK_RX";
    			adi,divider = <8>;	// 375
    			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS
    		};
    
    		hmc7044_c12: channel@12 {
    			reg = <12>;
    			adi,extended-name = "FPGA_REFCLK";
    			adi,divider = <8>;	// 375
    			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS
    		};
    
    		hmc7044_c13: channel@13 {
    			reg = <13>;
    			adi,extended-name = "FPGA_SYSREF";
    			adi,divider = <768>;	// 3.90625
    			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS
    			adi,jesd204-sysref-chan;
    		};
    	};
    };
    
    &fmc_spi {
    
    	trx0_ad9081: ad9081@0 {
    		#address-cells = <1>;
    		#size-cells = <0>;
    		compatible = "adi,ad9082";
    		reg = <0>;
    		spi-max-frequency = <5000000>;
    
    		/* Clocks */
    		clocks = <&hmc7044 2>;
    		clock-names = "dev_clk";
    
    		clock-output-names = "rx_sampl_clk", "tx_sampl_clk";
    		#clock-cells = <1>;
    
    		reset-gpios = <&axi_gpio 23 0>;
    		sysref-req-gpios = <&axi_gpio 11 0>;
    		rx2-enable-gpios = <&axi_gpio 25 0>;
    		rx1-enable-gpios = <&axi_gpio 24 0>;
    		tx2-enable-gpios = <&axi_gpio 27 0>;
    		tx1-enable-gpios = <&axi_gpio 26 0>;
    
    		jesd204-device;
    		#jesd204-cells = <2>;
    		jesd204-top-device = <0>; /* This is the TOP device */
    		jesd204-link-ids = <FRAMER_LINK0_RX DEFRAMER_LINK0_TX>;
    
    		jesd204-inputs =
    		<&axi_ad9081_core_rx 0 FRAMER_LINK0_RX>,
    		<&axi_ad9081_core_tx 0 DEFRAMER_LINK0_TX>;
    
    		adi,tx-dacs {
    			#size-cells = <0>;
    			#address-cells = <1>;
    			adi,dac-frequency-hz = /bits/ 64 <12000000000>;
    
    			adi,main-data-paths {
    				#address-cells = <1>;
    				#size-cells = <0>;
    				adi,interpolation = <2>;
    
    				ad9081_dac0: dac@0 {
    					reg = <0>;
    					adi,crossbar-select = <&ad9081_tx_fddc_chan0>;
    					adi,nco-frequency-shift-hz = /bits/ 64 <100000000>; /* 100 MHz */
    				};
    
    				ad9081_dac1: dac@1 {
    					reg = <1>;
    					adi,crossbar-select = <&ad9081_tx_fddc_chan1>;
    					adi,nco-frequency-shift-hz = /bits/ 64 <100000000>; /* 100 MHz */
    				};
    			};
    
    			adi,channelizer-paths {
    				#address-cells = <1>;
    				#size-cells = <0>;
    				adi,interpolation = <2>;
    
    				ad9081_tx_fddc_chan0: channel@0 {
    					reg = <0>;
    					adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
    					adi,nco-frequency-shift-hz =  /bits/ 64 <0>;
    				};
    
    				ad9081_tx_fddc_chan1: channel@1 {
    					reg = <1>;
    					adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
    					adi,nco-frequency-shift-hz =  /bits/ 64 <0>;
    				};
    			};
    
    			adi,jesd-links {
    				#size-cells = <0>;
    				#address-cells = <1>;
    
    				ad9081_tx_jesd_l0: link@0 {
    					#address-cells = <1>;
    					#size-cells = <0>;
    					reg = <0>;
    					adi,logical-lane-mapping = /bits/ 8 <0 2 7 6 1 5 4 3>;
    					adi,link-mode = <17>;			/* JESD Quick Configuration Mode */
    					adi,subclass = <1>;			/* JESD SUBCLASS 0,1,2 */
    					adi,version = <2>;			/* JESD VERSION 0=204A,1=204B,2=204C */
    					adi,dual-link = <0>;			/* JESD Dual Link Mode */
    					adi,converters-per-device = <4>;	/* JESD M */
    					adi,octets-per-frame = <1>;		/* JESD F */
    					adi,frames-per-multiframe = <256>;	/* JESD K */
    					adi,converter-resolution = <16>;	/* JESD N */
    					adi,bits-per-sample = <16>;		/* JESD NP' */
    					adi,control-bits-per-sample = <0>;	/* JESD CS */
    					adi,lanes-per-device = <8>;		/* JESD L */
    					adi,samples-per-converter-per-frame = <1>; /* JESD S */
    					adi,high-density = <1>;			/* JESD HD */
    
    					adi,tpl-phase-adjust = <0x3b>;
    				};
    			};
    		};
    
    		adi,rx-adcs {
    			#size-cells = <0>;
    			#address-cells = <1>;
    			adi,adc-frequency-hz = /bits/ 64 <6000000000>;
    
    			adi,main-data-paths {
    				#address-cells = <1>;
    				#size-cells = <0>;
    
    				ad9081_adc0: adc@0 {
    					reg = <0>;
    					adi,decimation = <2>;
    					adi,nco-frequency-shift-hz =  /bits/ 64 <100000000>;
    					adi,nco-mixer-mode = <AD9081_ADC_NCO_VIF>;
    				};
    
    				ad9081_adc1: adc@1 {
    					reg = <1>;
    					adi,decimation = <2>;
    					adi,nco-frequency-shift-hz =  /bits/ 64 <100000000>;
    					adi,nco-mixer-mode = <AD9081_ADC_NCO_VIF>;
    				};
    			};
    
    			adi,channelizer-paths {
    				#address-cells = <1>;
    				#size-cells = <0>;
    
    				ad9081_rx_fddc_chan0: channel@0 {
    					reg = <0>;
    					adi,decimation = <1>;
    					adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
    					adi,nco-frequency-shift-hz =  /bits/ 64 <0>;
    				};
    
    				ad9081_rx_fddc_chan1: channel@1 {
    					reg = <1>;
    					adi,decimation = <1>;
    					adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
    					adi,nco-frequency-shift-hz =  /bits/ 64 <0>;
    				};
    			};
    
    			adi,jesd-links {
    				#size-cells = <0>;
    				#address-cells = <1>;
    
    				ad9081_rx_jesd_l0: link@0 {
    					reg = <0>;
    					adi,converter-select =
    					<&ad9081_rx_fddc_chan0 FDDC_I>, <&ad9081_rx_fddc_chan0 FDDC_Q>,
    					<&ad9081_rx_fddc_chan1 FDDC_I>, <&ad9081_rx_fddc_chan1 FDDC_Q>;
    
    					adi,logical-lane-mapping = /bits/ 8 <2 0 7 6 5 4 3 1>;
    					adi,link-mode = <18>;			/* JESD Quick Configuration Mode */
    					adi,subclass = <1>;			/* JESD SUBCLASS 0,1,2 */
    					adi,version = <2>;			/* JESD VERSION 0=204A,1=204B,2=204C */
    					adi,dual-link = <0>;			/* JESD Dual Link Mode */
    					adi,converters-per-device = <4>;	/* JESD M */
    					adi,octets-per-frame = <1>;		/* JESD F */
    					adi,frames-per-multiframe = <256>;	/* JESD K */
    					adi,converter-resolution = <16>;	/* JESD N */
    					adi,bits-per-sample = <16>;		/* JESD NP' */
    					adi,control-bits-per-sample = <0>;	/* JESD CS */
    					adi,lanes-per-device = <8>;		/* JESD L */
    					adi,samples-per-converter-per-frame = <1>; /* JESD S */
    					adi,high-density = <1>;			/* JESD HD */
    				};
    			};
    		};
    
    	};
    };

    timing constraints:

    ###############################################################################
    ## Copyright (C) 2024-2024 Analog Devices, Inc. All rights reserved.
    ### SPDX short identifier: ADIBSD
    ###############################################################################
    
    # Primary clock definitions
    create_clock -name refclk         -period  2.667 [get_ports fpga_refclk_in_p]
    
    # device clock
    create_clock -name tx_device_clk  -period 2.667  [get_ports clkin6_p]
    create_clock -name rx_device_clk  -period 2.667  [get_ports clkin10_p]
    
    # Constraint SYSREFs
    # Assumption is that REFCLK and SYSREF have similar propagation delay,
    # and the SYSREF is a source synchronous Edge-Aligned signal to REFCLK
    set_input_delay -clock [get_clocks tx_device_clk] \
      [get_property PERIOD [get_clocks tx_device_clk]] \
      [get_ports {sysref2_*}]
    
    

    This is for the VPK120. Let me know if this helps, Thank you!

  • Thank you for sharing details. We'll look into the details and get back to you if we find anything.

  • Just to let you know that we have reproduced the issue and are still investing. It is not clear so far where the trouble is.

  • We found something interesting regarding your use case. If we apply the following slight modification to the settings, the DAC path works as expected, where the change to use 6 GHz DAC clock with 2x2 interpolation instead of 12 GHz with 2x1

    // SPDX-License-Identifier: GPL-2.0
    /*
     * Analog Devices AD9081-FMC-EBZ
     * https://wiki.analog.com/resources/tools-software/linux-drivers/iio-mxfe/ad9081
     * https://wiki.analog.com/resources/eval/user-guides/ad9081_fmca_ebz/ad9081_fmca_ebz_hdl
     *
     * hdl_project: <ad9081_fmca_ebz/vpk180>
     * board_revision: <>
     *
     * Copyright (C) 2019-2023 Analog Devices Inc.
     */
    
    #include "versal-vpk180-revA.dts"
    #include <dt-bindings/interrupt-controller/irq.h>
    #include <dt-bindings/iio/adc/adi,ad9081.h>
    #include <dt-bindings/jesd204/adxcvr.h>
    #include <dt-bindings/iio/frequency/hmc7044.h>
    							
    
    /* RX path */
    #define AD9081_RX_LANERATE_KHZ	24750000
    #define AD9081_RX_LINK_CLK	375000000
    
    /* TX path */
    #define AD9081_TX_LANERATE_KHZ	24750000
    #define AD9081_TX_LINK_CLK	375000000
    
    / {
    	model = "Analog Devices AD9081-FMC-EBZ-VPK180 Rev.A";
    
    	chosen {
    		bootargs = "console=ttyAMA0 earlycon=pl011,mmio32,0xFF000000,115200n8 clk_ignore_unused root=/dev/mmcblk0p2 rw rootfstype=ext4 rootwait";
    		stdout-path = "serial0:115200";
    	};
    
    	fpga_axi: fpga-axi@0 {
    		interrupt-parent = <&gic>;
    		compatible = "simple-bus";
    		#address-cells = <0x1>;
    		#size-cells = <0x1>;
    		ranges = <0 0 0 0xffffffff>;
    
    		clocks {
    			rx_fixed_linerate: clock@0 {
    				#clock-cells = <0>;
    				compatible = "fixed-clock";
    				clock-frequency = <AD9081_RX_LANERATE_KHZ>;
    				clock-output-names = "rx_lane_clk";
    			};
    
    			tx_fixed_linerate: clock@1 {
    				#clock-cells = <0>;
    				compatible = "fixed-clock";
    				clock-frequency = <AD9081_TX_LANERATE_KHZ>;
    				clock-output-names = "tx_lane_clk";
    			};
    
    			rx_fixed_link_clk: clock@2 {
    				#clock-cells = <0>;
    				compatible = "fixed-clock";
    				clock-frequency = <AD9081_RX_LINK_CLK>;
    				clock-output-names = "rx_link_clk";
    			};
    
    			tx_fixed_link_clk: clock@3 {
    				#clock-cells = <0>;
    				compatible = "fixed-clock";
    				clock-frequency = <AD9081_TX_LINK_CLK>;
    				clock-output-names = "tx_link_clk";
    			};
    		};
    
    		axi_gpio: gpio@a4000000 {
    			#gpio-cells = <2>;
    			#interrupt-cells = <2>;
    			clock-names = "s_axi_aclk";
    			clocks = <&versal_clk PMC_PL0_REF>;
    			compatible = "xlnx,axi-gpio-2.0", "xlnx,xps-gpio-1.00.a";
    			gpio-controller;
    			interrupt-controller;
    			interrupt-names = "ip2intc_irpt";
    			interrupt-parent = <&gic>;
    			interrupts = <0 84 4>;
    			reg = <0xa4000000 0x1000>;
    			xlnx,all-inputs = <0x0>;
    			xlnx,all-inputs-2 = <0x0>;
    			xlnx,all-outputs = <0x0>;
    			xlnx,all-outputs-2 = <0x0>;
    			xlnx,dout-default = <0x00000000>;
    			xlnx,dout-default-2 = <0x00000000>;
    			xlnx,gpio-width = <0x20>;
    			xlnx,gpio2-width = <0x20>;
    			xlnx,interrupt-present = <0x1>;
    			xlnx,is-dual = <0x1>;
    			xlnx,tri-default = <0xFFFFFFFF>;
    			xlnx,tri-default-2 = <0xFFFFFFFF>;
    		};
    
    		rx_dma: dma-controller@bc420000 {
    			compatible = "adi,axi-dmac-1.00.a";
    			reg = <0xbc420000 0x10000>;
    			#dma-cells = <1>;
    			#clock-cells = <0>;
    			interrupts = <0 97 IRQ_TYPE_LEVEL_HIGH>;
    			clocks = <&versal_clk PMC_PL1_REF>;
    		};
    
    		tx_dma: dma-controller@bc430000 {
    			compatible = "adi,axi-dmac-1.00.a";
    			reg = <0xbc430000 0x10000>;
    			#dma-cells = <1>;
    			#clock-cells = <0>;
    			interrupts = <0 96 IRQ_TYPE_LEVEL_HIGH>;
    			clocks = <&versal_clk PMC_PL1_REF>;
    		};
    
    		axi_ad9081_core_rx: axi-ad9081-rx-hpc@a4a10000 {
    			compatible = "adi,axi-ad9081-rx-1.0";
    			reg = <0xa4a10000 0x8000>;
    			dmas = <&rx_dma 0>;
    			dma-names = "rx";
    			spibus-connected = <&trx0_ad9081>;
    
    			jesd204-device;
    			#jesd204-cells = <2>;
    			jesd204-inputs = <&axi_ad9081_rx_jesd 0 FRAMER_LINK0_RX>;
    		};
    
    		axi_ad9081_core_tx: axi-ad9081-tx-hpc@a4b10000 {
    			compatible = "adi,axi-ad9081-tx-1.0";
    			reg = <0xa4b10000 0x4000>;
    			dmas = <&tx_dma 0>;
    			dma-names = "tx";
    			clocks = <&trx0_ad9081 1>;
    			clock-names = "sampl_clk";
    			spibus-connected = <&trx0_ad9081>;
    
    			jesd204-device;
    			#jesd204-cells = <2>;
    			jesd204-inputs = <&axi_ad9081_tx_jesd 0 DEFRAMER_LINK0_TX>;
    		};
    
    		axi_ad9081_rx_jesd: axi-jesd204-rx@a4a90000 {
    			compatible = "adi,axi-jesd204-rx-1.0";
    			reg = <0xa4a90000 0x1000>;
    
    			interrupts = <0 95 IRQ_TYPE_LEVEL_HIGH>;
    
    			clocks = <&versal_clk PMC_PL0_REF>, <&hmc7044 10>, <&rx_fixed_link_clk>, <&rx_fixed_linerate>;
    			clock-names = "s_axi_aclk", "device_clk", "link_clk", "lane_clk";
    
    			#clock-cells = <0>;
    			clock-output-names = "jesd_rx_lane_clk";
    
    			jesd204-device;
    			#jesd204-cells = <2>;
    			jesd204-inputs = <&hmc7044 0 FRAMER_LINK0_RX>;
    
    			reset-done-gpios = <&axi_gpio 32 0>;
    			pll-datapath-reset-gpios = <&axi_gpio 36 0>;
    			datapath-reset-gpios = <&axi_gpio 38 0>;
    		};
    
    		axi_ad9081_tx_jesd: axi-jesd204-tx@a4b90000 {
    			compatible = "adi,axi-jesd204-tx-1.0";
    			reg = <0xa4b90000 0x1000>;
    
    			interrupts = <0 94 IRQ_TYPE_LEVEL_HIGH>;
    
    			clocks = <&versal_clk PMC_PL0_REF>, <&hmc7044 6>, <&tx_fixed_link_clk>, <&tx_fixed_linerate>;
    			clock-names = "s_axi_aclk", "device_clk", "link_clk", "lane_clk";
    
    			#clock-cells = <0>;
    			clock-output-names = "jesd_tx_lane_clk";
    
    			jesd204-device;
    			#jesd204-cells = <2>;
    			jesd204-inputs = <&hmc7044 0 DEFRAMER_LINK0_TX>;
    
    			reset-done-gpios = <&axi_gpio 33 0>;
    			pll-datapath-reset-gpios = <&axi_gpio 37 0>;
    			datapath-reset-gpios = <&axi_gpio 39 0>;
    		};
    
    		axi_sysid_0: axi-sysid-0@a5000000 {
    			compatible = "adi,axi-sysid-1.00.a";
    			reg = <0xa5000000 0x10000>;
    		};
    	};
    };
    
    &gic {
    	num_cpus = <2>;
    	num_interrupts = <96>;
    };
    
    &lpd_dma_chan0 {
    	status = "okay";
    };
    
    &lpd_dma_chan1 {
    	status = "okay";
    };
    
    &lpd_dma_chan2 {
    	status = "okay";
    };
    
    &lpd_dma_chan3 {
    	status = "okay";
    };
    
    &lpd_dma_chan4 {
    	status = "okay";
    };
    
    &lpd_dma_chan5 {
    	status = "okay";
    };
    
    &lpd_dma_chan6 {
    	status = "okay";
    };
    
    &lpd_dma_chan7 {
    	status = "okay";
    };
    
    &cci {
    	status = "okay";
    };
    
    &smmu {
    	status = "okay";
    };
    
    &i2c1 {
    	status = "disabled";
    };
    
    &gpio1 {
    	status = "okay";
    };
    
    &qspi {
    	is-dual = <1>;
    	num-cs = <1>;
    	spi-rx-bus-width = <4>;
    	spi-tx-bus-width = <4>;
    	status = "okay";
    };
    
    &sdhci1 {
    	clock-frequency = <199999985>;
    	status = "okay";
    };
    
    &serial0 {
    	cts-override ;
    	device_type = "serial";
    	port-number = <0>;
    };
    
    &spi0 {
    	is-decoded-cs = <0>;
    	num-cs = <3>;
    	status = "okay";
    };
    
    &spi1 {
    	is-decoded-cs = <0>;
    	num-cs = <3>;
    	status = "okay";
    };
    
    &ttc0 {
    	status = "okay";
    };
    
    &ref {
    	clock-frequency = <33333333>;
    };
    
    &gem0 {
    	local-mac-address = [00 0a 35 ad 90 81];
    };
    
    &fpga_axi {
    	axi_data_offload_tx: axi-data-offload-0@bc440000 {
    		compatible = "adi,axi-data-offload-1.0.a";
    		reg = <0xbc440000 0x10000>;
    	};
    
    	axi_data_offload_rx: axi-data-offload-1@bc450000 {
    		compatible = "adi,axi-data-offload-1.0.a";
    		reg = <0xbc450000 0x10000>;
    	};
    };
    
    &axi_ad9081_core_tx {
    	adi,axi-data-offload-connected = <&axi_data_offload_tx>;
    	adi,axi-pl-fifo-enable;
    };
    
    #define fmc_spi spi0
    
    &spi1 {
    	status = "okay";
    
    	hmc7044: hmc7044@0 {
    		#address-cells = <1>;
    		#size-cells = <0>;
    		#clock-cells = <1>;
    		compatible = "adi,hmc7044";
    		reg = <0>;
    		spi-max-frequency = <1000000>;
    
    		jesd204-device;
    		#jesd204-cells = <2>;
    		jesd204-sysref-provider;
    
    		adi,jesd204-max-sysref-frequency-hz = <2000000>; /* 2 MHz */
    
    		/*
    		 * There are different versions of the AD9081-FMCA-EBZ & AD9082-FMCA-EBZ
    		 * VCXO = 122.880 MHz, XO = 122.880MHz (AD9081-FMC-EBZ & AD9082-FMC-EBZ)
    		 * VCXO = 100.000 MHz, XO = 100.000MHz (AD9081-FMC-EBZ-A2 & AD9082-FMC-EBZ-A2)
    		 * To determine which board is which, read the freqency printed on the VCXO
    		 * or use the fru-dump utility:
    		 * #fru-dump -b /sys/bus/i2c/devices/15-0050/eeprom
    		 */
    
    		//adi,pll1-clkin-frequencies = <122880000 30720000 0 0>;
    		//adi,vcxo-frequency = <122880000>;
    
    		adi,pll1-clkin-frequencies = <100000000 10000000 0 0>;
    		adi,pll1-ref-prio-ctrl = <0xE1>; /* prefer CLKIN1 -> CLKIN0 -> CLKIN2 -> CLKIN3 */
    		adi,pll1-ref-autorevert-enable;
    		adi,vcxo-frequency = <100000000>;
    
    		adi,pll1-loop-bandwidth-hz = <200>;
    		adi,pll1-charge-pump-current-ua = <720>;
    		adi,pfd1-maximum-limit-frequency-hz = <1000000>; /* 1 MHz */
    
    		adi,pll2-output-frequency = <3000000000>;
    
    		adi,sysref-timer-divider = <1024>;
    		adi,pulse-generator-mode = <0>;
    
    		adi,clkin0-buffer-mode  = <0x07>;
    		adi,clkin1-buffer-mode  = <0x07>;
    		adi,oscin-buffer-mode = <0x15>;
    
    		adi,gpi-controls = <0x00 0x00 0x00 0x00>;
    		adi,gpo-controls = <0x37 0x33 0x00 0x00>;
    
    		clock-output-names =
    		"hmc7044_out0", "hmc7044_out1", "hmc7044_out2",
    		"hmc7044_out3", "hmc7044_out4", "hmc7044_out5",
    		"hmc7044_out6", "hmc7044_out7", "hmc7044_out8",
    		"hmc7044_out9", "hmc7044_out10", "hmc7044_out11",
    		"hmc7044_out12", "hmc7044_out13";
    
    		hmc7044_c0: channel@0 {
    			reg = <0>;
    			adi,extended-name = "CORE_CLK_RX";
    			adi,divider = <8>;	// 375
    			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS
    
    		};
    
    		hmc7044_c2: channel@2 {
    			reg = <2>;
    			adi,extended-name = "DEV_REFCLK";
    			adi,divider = <8>;	// 375
    			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS
    		};
    
    		hmc7044_c3: channel@3 {
    			reg = <3>;
    			adi,extended-name = "DEV_SYSREF";
    			adi,divider = <768>;	// 3.90625
    			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS
    			adi,jesd204-sysref-chan;
    		};
    
    		hmc7044_c6: channel@6 {
    			reg = <6>;
    			adi,extended-name = "CORE_CLK_TX";
    			adi,divider = <8>;	// 250 = LR/66*4/6
    			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS
    		};
    
    		hmc7044_c8: channel@8 {
    			reg = <8>;
    			adi,extended-name = "FPGA_REFCLK1";
    			adi,divider = <8>;	// 750
    			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS
    		};
    
    		hmc7044_c10: channel@10 {
    			reg = <10>;
    			adi,extended-name = "CORE_CLK_RX";
    			adi,divider = <8>;	// 250 = LR/66*4/6
    			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS
    		};
    
    		hmc7044_c12: channel@12 {
    			reg = <12>;
    			adi,extended-name = "FPGA_REFCLK";
    			adi,divider = <8>;	// 375
    			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS
    		};
    
    		hmc7044_c13: channel@13 {
    			reg = <13>;
    			adi,extended-name = "FPGA_SYSREF";
    			adi,divider = <768>;	// 3.90625
    			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS
    			adi,jesd204-sysref-chan;
    		};
    	};
    };
    
    &fmc_spi {
    
    	trx0_ad9081: ad9081@0 {
    		#address-cells = <1>;
    		#size-cells = <0>;
    		compatible = "adi,ad9081";
    		reg = <0>;
    		spi-max-frequency = <5000000>;
    
    		/* Clocks */
    		clocks = <&hmc7044 2>;
    		clock-names = "dev_clk";
    
    		clock-output-names = "rx_sampl_clk", "tx_sampl_clk";
    		#clock-cells = <1>;
    
    		reset-gpios = <&axi_gpio 23 0>;
    		sysref-req-gpios = <&axi_gpio 11 0>;
    		rx2-enable-gpios = <&axi_gpio 25 0>;
    		rx1-enable-gpios = <&axi_gpio 24 0>;
    		tx2-enable-gpios = <&axi_gpio 27 0>;
    		tx1-enable-gpios = <&axi_gpio 26 0>;
    
    		jesd204-device;
    		#jesd204-cells = <2>;
    		jesd204-top-device = <0>; /* This is the TOP device */
    		jesd204-link-ids = <FRAMER_LINK0_RX DEFRAMER_LINK0_TX>;
    
    		jesd204-inputs =
    		<&axi_ad9081_core_rx 0 FRAMER_LINK0_RX>,
    		<&axi_ad9081_core_tx 0 DEFRAMER_LINK0_TX>;
    
    		adi,tx-dacs {
    			#size-cells = <0>;
    			#address-cells = <1>;
    			adi,dac-frequency-hz = /bits/ 64 <6000000000>;
    
    			adi,main-data-paths {
    				#address-cells = <1>;
    				#size-cells = <0>;
    				adi,interpolation = <2>;
    
    				ad9081_dac0: dac@0 {
    					reg = <0>;
    					adi,crossbar-select = <&ad9081_tx_fddc_chan0>;
    					adi,nco-frequency-shift-hz = /bits/ 64 <1000000000>; /* 100 MHz */
    				};
    
    				ad9081_dac1: dac@1 {
    					reg = <1>;
    					adi,crossbar-select = <&ad9081_tx_fddc_chan1>;
    					adi,nco-frequency-shift-hz = /bits/ 64 <1000000000>; /* 1100 MHz */
    				};
    
    				// ad9081_dac2: dac@2 {
    				// 	reg = <2>;
    				// 	adi,crossbar-select = <&ad9081_tx_fddc_chan2>; /* All 4 channels @ dac2 */
    				// 	adi,nco-frequency-shift-hz = /bits/ 64 <1200000000>;  /* 300 MHz */
    				// };
    
    				// ad9081_dac3: dac@3 {
    				// 	reg = <3>;
    				// 	adi,crossbar-select = <&ad9081_tx_fddc_chan3>; /* All 4 channels @ dac2 */
    				// 	adi,nco-frequency-shift-hz = /bits/ 64 <1300000000>; /* 400 MHz */
    				// };
    			};
    
    			adi,channelizer-paths {
    				#address-cells = <1>;
    				#size-cells = <0>;
    				adi,interpolation = <1>;
    
    				ad9081_tx_fddc_chan0: channel@0 {
    					reg = <0>;
    					adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
    					adi,nco-frequency-shift-hz =  /bits/ 64 <0>;
    				};
    
    				ad9081_tx_fddc_chan1: channel@1 {
    					reg = <1>;
    					adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
    					adi,nco-frequency-shift-hz =  /bits/ 64 <0>;
    				};
    
    				// ad9081_tx_fddc_chan2: channel@2 {
    				// 	reg = <2>;
    				// 	adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
    				// 	adi,nco-frequency-shift-hz =  /bits/ 64 <0>;
    				// };
    
    				// ad9081_tx_fddc_chan3: channel@3 {
    				// 	reg = <3>;
    				// 	adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
    				// 	adi,nco-frequency-shift-hz =  /bits/ 64 <0>;
    				// };
    			};
    
    			adi,jesd-links {
    				#size-cells = <0>;
    				#address-cells = <1>;
    
    				ad9081_tx_jesd_l0: link@0 {
    					#address-cells = <1>;
    					#size-cells = <0>;
    					reg = <0>;
    					adi,logical-lane-mapping = /bits/ 8 <0 2 7 6 1 5 4 3>;
    					adi,link-mode = <17>;			/* JESD Quick Configuration Mode */
    					adi,subclass = <1>;			/* JESD SUBCLASS 0,1,2 */
    					adi,version = <2>;			/* JESD VERSION 0=204A,1=204B,2=204C */
    					adi,dual-link = <0>;			/* JESD Dual Link Mode */
    					adi,converters-per-device = <4>;	/* JESD M */
    					adi,octets-per-frame = <1>;		/* JESD F */
    					adi,frames-per-multiframe = <256>;	/* JESD K */
    					adi,converter-resolution = <16>;	/* JESD N */
    					adi,bits-per-sample = <16>;		/* JESD NP' */
    					adi,control-bits-per-sample = <0>;	/* JESD CS */
    					adi,lanes-per-device = <8>;		/* JESD L */
    					adi,samples-per-converter-per-frame = <1>; /* JESD S */
    					adi,high-density = <1>;			/* JESD HD */
    
    					adi,tpl-phase-adjust = <0x3>;
    				};
    			};
    		};
    
    		adi,rx-adcs {
    			#size-cells = <0>;
    			#address-cells = <1>;
    			adi,adc-frequency-hz = /bits/ 64 <6000000000>;
    
    			adi,main-data-paths {
    				#address-cells = <1>;
    				#size-cells = <0>;
    
    				ad9081_adc0: adc@0 {
    					reg = <0>;
    					adi,decimation = <2>;
    					adi,nco-frequency-shift-hz =  /bits/ 64 <100000000>;
    					adi,nco-mixer-mode = <AD9081_ADC_NCO_VIF>;
    				};
    
    				ad9081_adc1: adc@1 {
    					reg = <1>;
    					adi,decimation = <2>;
    					adi,nco-frequency-shift-hz =  /bits/ 64 <100000000>;
    					adi,nco-mixer-mode = <AD9081_ADC_NCO_VIF>;
    				};
    
    				// ad9081_adc2: adc@2 {
    				// 	reg = <2>;
    				// 	adi,decimation = <1>;
    				// 	adi,nco-frequency-shift-hz =  /bits/ 64 <100000000>;
    				// 	adi,nco-mixer-mode = <AD9081_ADC_NCO_VIF>;
    				// };
    
    				// ad9081_adc3: adc@3 {
    				// 	reg = <3>;
    				// 	adi,decimation = <1>;
    				// 	adi,nco-frequency-shift-hz =  /bits/ 64 <100000000>;
    				// 	adi,nco-mixer-mode = <AD9081_ADC_NCO_VIF>;
    				// };
    			};
    
    			adi,channelizer-paths {
    				#address-cells = <1>;
    				#size-cells = <0>;
    
    				ad9081_rx_fddc_chan0: channel@0 {
    					reg = <0>;
    					adi,decimation = <1>;
    					adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
    					adi,nco-frequency-shift-hz =  /bits/ 64 <0>;
    				};
    
    				ad9081_rx_fddc_chan1: channel@1 {
    					reg = <1>;
    					adi,decimation = <1>;
    					adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
    					adi,nco-frequency-shift-hz =  /bits/ 64 <0>;
    				};
    
    				// ad9081_rx_fddc_chan4: channel@4 {
    				// 	reg = <4>;
    				// 	adi,decimation = <1>;
    				// 	adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
    				// 	adi,nco-frequency-shift-hz =  /bits/ 64 <0>;
    				// };
    
    				// ad9081_rx_fddc_chan5: channel@5 {
    				// 	reg = <5>;
    				// 	adi,decimation = <1>;
    				// 	adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
    				// 	adi,nco-frequency-shift-hz =  /bits/ 64 <0>;
    				// };
    			};
    
    			adi,jesd-links {
    				#size-cells = <0>;
    				#address-cells = <1>;
    
    				ad9081_rx_jesd_l0: link@0 {
    					reg = <0>;
    					adi,converter-select =
    					<&ad9081_rx_fddc_chan0 FDDC_I>, <&ad9081_rx_fddc_chan0 FDDC_Q>,
    					<&ad9081_rx_fddc_chan1 FDDC_I>, <&ad9081_rx_fddc_chan1 FDDC_Q>;
    					// <&ad9081_rx_fddc_chan4 FDDC_I>, <&ad9081_rx_fddc_chan4 FDDC_Q>,
    					// <&ad9081_rx_fddc_chan5 FDDC_I>, <&ad9081_rx_fddc_chan5 FDDC_Q>;
    					adi,logical-lane-mapping = /bits/ 8 <2 0 7 6 5 4 3 1>;
    					adi,link-mode = <18>;			/* JESD Quick Configuration Mode */
    					adi,subclass = <1>;			/* JESD SUBCLASS 0,1,2 */
    					adi,version = <2>;			/* JESD VERSION 0=204A,1=204B,2=204C */
    					adi,dual-link = <0>;			/* JESD Dual Link Mode */
    					adi,converters-per-device = <4>;	/* JESD M */
    					adi,octets-per-frame = <1>;		/* JESD F */
    					adi,frames-per-multiframe = <256>;	/* JESD K */
    					adi,converter-resolution = <16>;	/* JESD N */
    					adi,bits-per-sample = <16>;		/* JESD NP' */
    					adi,control-bits-per-sample = <0>;	/* JESD CS */
    					adi,lanes-per-device = <8>;		/* JESD L */
    					adi,samples-per-converter-per-frame = <1>; /* JESD S */
    					adi,high-density = <1>;			/* JESD HD */
    				};
    			};
    		};
    
    	};
    };
    

    This confirms that the HDL is not the source of the problem; the issue is most likely related to the software driver that configures the chip. We will continue our investigation. In the meantime, could you please change your DAC clock and interpolation to 6 GHz and 2x1, respectively, to confirm our observations

    -YH

  • Hello! thank you for the suggestions, your help is invaluable. I changed the device tree to the following with your suggested change:

    #include <dt-bindings/gpio/gpio.h>
    #include <dt-bindings/iio/frequency/hmc7044.h>
    #include <dt-bindings/iio/adc/adi,ad9081.h>
    #include <dt-bindings/interrupt-controller/irq.h>
    #include <dt-bindings/jesd204/adxcvr.h>
    
    /include/ "system-conf.dtsi"
    
    /* RX path */
    #define AD9081_RX_LANERATE_KHZ	24750000
    #define AD9081_RX_LINK_CLK	375000000
    
    /* TX path */
    #define AD9081_TX_LANERATE_KHZ	24750000
    #define AD9081_TX_LINK_CLK	375000000
    
    / {
    	model = "Analog Devices AD9081-FMC-EBZ-VPK180 Rev.A";
    
    	chosen {
    		bootargs = "console=ttyAMA0 earlycon=pl011,mmio32,0xFF000000,115200n8 clk_ignore_unused root=/dev/mmcblk0p2 rw rootfstype=ext4 rootwait";
    		stdout-path = "serial0:115200";
    	};
    
    	fpga_axi: fpga-axi@0 {
    		interrupt-parent = <&gic>;
    		compatible = "simple-bus";
    		#address-cells = <0x1>;
    		#size-cells = <0x1>;
    		ranges = <0 0 0 0xffffffff>;
    
    		clocks {
    			rx_fixed_linerate: clock@0 {
    				#clock-cells = <0>;
    				compatible = "fixed-clock";
    				clock-frequency = <AD9081_RX_LANERATE_KHZ>;
    				clock-output-names = "rx_lane_clk";
    			};
    
    			tx_fixed_linerate: clock@1 {
    				#clock-cells = <0>;
    				compatible = "fixed-clock";
    				clock-frequency = <AD9081_TX_LANERATE_KHZ>;
    				clock-output-names = "tx_lane_clk";
    			};
    
    			rx_fixed_link_clk: clock@2 {
    				#clock-cells = <0>;
    				compatible = "fixed-clock";
    				clock-frequency = <AD9081_RX_LINK_CLK>;
    				clock-output-names = "rx_link_clk";
    			};
    
    			tx_fixed_link_clk: clock@3 {
    				#clock-cells = <0>;
    				compatible = "fixed-clock";
    				clock-frequency = <AD9081_TX_LINK_CLK>;
    				clock-output-names = "tx_link_clk";
    			};
    		};
    
    		axi_gpio: gpio@a4000000 {
    			#gpio-cells = <2>;
    			#interrupt-cells = <2>;
    			clock-names = "s_axi_aclk";
    			clocks = <&versal_clk PMC_PL0_REF>;
    			compatible = "xlnx,axi-gpio-2.0", "xlnx,xps-gpio-1.00.a";
    			gpio-controller;
    			interrupt-controller;
    			interrupt-names = "ip2intc_irpt";
    			interrupt-parent = <&gic>;
    			interrupts = <0 84 4>;
    			reg = <0xa4000000 0x1000>;
    			xlnx,all-inputs = <0x0>;
    			xlnx,all-inputs-2 = <0x0>;
    			xlnx,all-outputs = <0x0>;
    			xlnx,all-outputs-2 = <0x0>;
    			xlnx,dout-default = <0x00000000>;
    			xlnx,dout-default-2 = <0x00000000>;
    			xlnx,gpio-width = <0x20>;
    			xlnx,gpio2-width = <0x20>;
    			xlnx,interrupt-present = <0x1>;
    			xlnx,is-dual = <0x1>;
    			xlnx,tri-default = <0xFFFFFFFF>;
    			xlnx,tri-default-2 = <0xFFFFFFFF>;
    		};
    
    		rx_dma: dma@bc420000 {
    			compatible = "adi,axi-dmac-1.00.a";
    			reg = <0xbc420000 0x10000>;
    			#dma-cells = <1>;
    			#clock-cells = <0>;
    			interrupts = <0 97 IRQ_TYPE_LEVEL_HIGH>;
    			clocks = <&versal_clk PMC_PL1_REF>;
    		};
    
    		tx_dma: dma@bc430000  {
    			compatible = "adi,axi-dmac-1.00.a";
    			reg = <0xbc430000 0x10000>;
    			#dma-cells = <1>;
    			#clock-cells = <0>;
    			interrupts = <0 96 IRQ_TYPE_LEVEL_HIGH>;
    			clocks = <&versal_clk PMC_PL1_REF>;
    		};
    
    		axi_ad9081_core_rx: axi-ad9081-rx-hpc@a4a10000 {
    			compatible = "adi,axi-ad9081-rx-1.0";
    			reg = <0xa4a10000 0x8000>;
    			dmas = <&rx_dma 0>;
    			dma-names = "rx";
    			spibus-connected = <&trx0_ad9081>;
    
    			jesd204-device;
    			#jesd204-cells = <2>;
    			jesd204-inputs = <&axi_ad9081_rx_jesd 0 FRAMER_LINK0_RX>;
    		};
    
    		axi_ad9081_core_tx: axi-ad9081-tx-hpc@a4b10000 {
    			compatible = "adi,axi-ad9081-tx-1.0";
    			reg = <0xa4b10000 0x4000>;
    			dmas = <&tx_dma 0>;
    			dma-names = "tx";
    			clocks = <&trx0_ad9081 1>;
    			clock-names = "sampl_clk";
    			spibus-connected = <&trx0_ad9081>;
    
    			jesd204-device;
    			#jesd204-cells = <2>;
    			jesd204-inputs = <&axi_ad9081_tx_jesd 0 DEFRAMER_LINK0_TX>;
    		};
    
    		axi_ad9081_rx_jesd: axi-jesd204-rx@a4a90000 {
    			compatible = "adi,axi-jesd204-rx-1.0";
    			reg = <0xa4a90000 0x1000>;
    
    			interrupts = <0 95 IRQ_TYPE_LEVEL_HIGH>;
    
    			clocks = <&versal_clk PMC_PL0_REF>, <&hmc7044 10>, <&rx_fixed_link_clk>, <&rx_fixed_linerate>;
    			clock-names = "s_axi_aclk", "device_clk", "link_clk", "lane_clk";
    
    			#clock-cells = <0>;
    			clock-output-names = "jesd_rx_lane_clk";
    
    			jesd204-device;
    			#jesd204-cells = <2>;
    			jesd204-inputs = <&hmc7044 0 FRAMER_LINK0_RX>;
    
    			reset-done-gpios = <&axi_gpio 32 0>;
    			pll-datapath-reset-gpios = <&axi_gpio 36 0>;
    			datapath-reset-gpios = <&axi_gpio 38 0>;
    		};
    
    		axi_ad9081_tx_jesd: axi-jesd204-tx@a4b90000 {
    			compatible = "adi,axi-jesd204-tx-1.0";
    			reg = <0xa4b90000 0x1000>;
    
    			interrupts = <0 94 IRQ_TYPE_LEVEL_HIGH>;
    
    			clocks = <&versal_clk PMC_PL0_REF>, <&hmc7044 6>, <&tx_fixed_link_clk>, <&tx_fixed_linerate>;
    			clock-names = "s_axi_aclk", "device_clk", "link_clk", "lane_clk";
    
    			#clock-cells = <0>;
    			clock-output-names = "jesd_tx_lane_clk";
    
    			jesd204-device;
    			#jesd204-cells = <2>;
    			jesd204-inputs = <&hmc7044 0 DEFRAMER_LINK0_TX>;
    
    			reset-done-gpios = <&axi_gpio 33 0>;
    			pll-datapath-reset-gpios = <&axi_gpio 37 0>;
    			datapath-reset-gpios = <&axi_gpio 39 0>;
    		};
    
    		axi_sysid_0: axi-sysid-0@a5000000 {
    			compatible = "adi,axi-sysid-1.00.a";
    			reg = <0xa5000000 0x10000>;
    		};
    	};
    };
    
    &gic {
    	num_cpus = <2>;
    	num_interrupts = <96>;
    };
    
    &lpd_dma_chan0 {
    	status = "okay";
    };
    
    &lpd_dma_chan1 {
    	status = "okay";
    };
    
    &lpd_dma_chan2 {
    	status = "okay";
    };
    
    &lpd_dma_chan3 {
    	status = "okay";
    };
    
    &lpd_dma_chan4 {
    	status = "okay";
    };
    
    &lpd_dma_chan5 {
    	status = "okay";
    };
    
    &lpd_dma_chan6 {
    	status = "okay";
    };
    
    &lpd_dma_chan7 {
    	status = "okay";
    };
    
    &cci {
    	status = "okay";
    };
    
    &smmu {
    	status = "okay";
    };
    
    &i2c1 {
    	status = "disabled";
    };
    
    &gpio1 {
    	status = "okay";
    };
    
    &qspi {
    	is-dual = <1>;
    	num-cs = <1>;
    	spi-rx-bus-width = <4>;
    	spi-tx-bus-width = <4>;
    	status = "okay";
    };
    
    &sdhci1 {
    	clock-frequency = <199999985>;
    	status = "okay";
    };
    
    &serial0 {
    	cts-override ;
    	device_type = "serial";
    	port-number = <0>;
    };
    
    &spi0 {
    	is-decoded-cs = <0>;
    	num-cs = <3>;
    	status = "okay";
    };
    
    &spi1 {
    	is-decoded-cs = <0>;
    	num-cs = <3>;
    	status = "okay";
    };
    
    &ttc0 {
    	status = "okay";
    };
    
    &ref_clk {
    	clock-frequency = <33333333>;
    };
    
    &gem0 {
    	local-mac-address = [00 0a 35 ad 90 81];
    };
    
    &fpga_axi {
    	axi_data_offload_tx: axi-data-offload-0@bc440000 {
    		compatible = "adi,axi-data-offload-1.0.a";
    		reg = <0xbc440000 0x10000>;
    	};
    
    	axi_data_offload_rx: axi-data-offload-1@bc450000 {
    		compatible = "adi,axi-data-offload-1.0.a";
    		reg = <0xbc450000 0x10000>;
    	};
    };
    
    &axi_ad9081_core_tx {
    	adi,axi-data-offload-connected = <&axi_data_offload_tx>;
    	adi,axi-pl-fifo-enable;
    };
    
    #define fmc_spi spi0
    
    &spi1 {
    	status = "okay";
    
    	hmc7044: hmc7044@0 {
    		#address-cells = <1>;
    		#size-cells = <0>;
    		#clock-cells = <1>;
    		compatible = "adi,hmc7044";
    		reg = <0>;
    		spi-max-frequency = <1000000>;
    
    		jesd204-device;
    		#jesd204-cells = <2>;
    		jesd204-sysref-provider;
    
    		adi,jesd204-max-sysref-frequency-hz = <2000000>; /* 2 MHz */
    
    		/*
    		 * There are different versions of the AD9081-FMCA-EBZ & AD9082-FMCA-EBZ
    		 * VCXO = 122.880 MHz, XO = 122.880MHz (AD9081-FMC-EBZ & AD9082-FMC-EBZ)
    		 * VCXO = 100.000 MHz, XO = 100.000MHz (AD9081-FMC-EBZ-A2 & AD9082-FMC-EBZ-A2)
    		 * To determine which board is which, read the freqency printed on the VCXO
    		 * or use the fru-dump utility:
    		 * #fru-dump -b /sys/bus/i2c/devices/15-0050/eeprom
    		 */
    
    		//adi,pll1-clkin-frequencies = <122880000 30720000 0 0>;
    		//adi,vcxo-frequency = <122880000>;
    
    		adi,pll1-clkin-frequencies = <100000000 10000000 0 0>;
    		adi,pll1-ref-prio-ctrl = <0xE1>; /* prefer CLKIN1 -> CLKIN0 -> CLKIN2 -> CLKIN3 */
    		adi,pll1-ref-autorevert-enable;
    		adi,vcxo-frequency = <100000000>;
    
    		adi,pll1-loop-bandwidth-hz = <200>;
    		adi,pll1-charge-pump-current-ua = <720>;
    		adi,pfd1-maximum-limit-frequency-hz = <1000000>; /* 1 MHz */
    
    		adi,pll2-output-frequency = <3000000000>;
    
    		adi,sysref-timer-divider = <1024>;
    		adi,pulse-generator-mode = <0>;
    
    		adi,clkin0-buffer-mode  = <0x07>;
    		adi,clkin1-buffer-mode  = <0x07>;
    		adi,oscin-buffer-mode = <0x15>;
    
    		adi,gpi-controls = <0x00 0x00 0x00 0x00>;
    		adi,gpo-controls = <0x37 0x33 0x00 0x00>;
    
    		clock-output-names =
    		"hmc7044_out0", "hmc7044_out1", "hmc7044_out2",
    		"hmc7044_out3", "hmc7044_out4", "hmc7044_out5",
    		"hmc7044_out6", "hmc7044_out7", "hmc7044_out8",
    		"hmc7044_out9", "hmc7044_out10", "hmc7044_out11",
    		"hmc7044_out12", "hmc7044_out13";
    
    		hmc7044_c0: channel@0 {
    			reg = <0>;
    			adi,extended-name = "CORE_CLK_RX";
    			adi,divider = <8>;	// 375
    			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS
    
    		};
    
    		hmc7044_c2: channel@2 {
    			reg = <2>;
    			adi,extended-name = "DEV_REFCLK";
    			adi,divider = <8>;	// 375
    			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS
    		};
    
    		hmc7044_c3: channel@3 {
    			reg = <3>;
    			adi,extended-name = "DEV_SYSREF";
    			adi,divider = <768>;	// 3.90625
    			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS
    			adi,jesd204-sysref-chan;
    		};
    
    		hmc7044_c6: channel@6 {
    			reg = <6>;
    			adi,extended-name = "CORE_CLK_TX";
    			adi,divider = <8>;	// 375
    			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS
    		};
    
    		hmc7044_c8: channel@8 {
    			reg = <8>;
    			adi,extended-name = "FPGA_REFCLK1";
    			adi,divider = <8>;	// 375
    			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS
    		};
    
    		hmc7044_c10: channel@10 {
    			reg = <10>;
    			adi,extended-name = "CORE_CLK_RX";
    			adi,divider = <8>;	// 375
    			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS
    		};
    
    		hmc7044_c12: channel@12 {
    			reg = <12>;
    			adi,extended-name = "FPGA_REFCLK";
    			adi,divider = <8>;	// 375
    			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS
    		};
    
    		hmc7044_c13: channel@13 {
    			reg = <13>;
    			adi,extended-name = "FPGA_SYSREF";
    			adi,divider = <768>;	// 3.90625
    			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS
    			adi,jesd204-sysref-chan;
    		};
    	};
    };
    
    &fmc_spi {
    
    	trx0_ad9081: ad9081@0 {
    		#address-cells = <1>;
    		#size-cells = <0>;
    		compatible = "adi,ad9082";
    		reg = <0>;
    		spi-max-frequency = <5000000>;
    
    		/* Clocks */
    		clocks = <&hmc7044 2>;
    		clock-names = "dev_clk";
    
    		clock-output-names = "rx_sampl_clk", "tx_sampl_clk";
    		#clock-cells = <1>;
    
    		reset-gpios = <&axi_gpio 23 0>;
    		sysref-req-gpios = <&axi_gpio 11 0>;
    		rx2-enable-gpios = <&axi_gpio 25 0>;
    		rx1-enable-gpios = <&axi_gpio 24 0>;
    		tx2-enable-gpios = <&axi_gpio 27 0>;
    		tx1-enable-gpios = <&axi_gpio 26 0>;
    
    		jesd204-device;
    		#jesd204-cells = <2>;
    		jesd204-top-device = <0>; /* This is the TOP device */
    		jesd204-link-ids = <FRAMER_LINK0_RX DEFRAMER_LINK0_TX>;
    
    		jesd204-inputs =
    		<&axi_ad9081_core_rx 0 FRAMER_LINK0_RX>,
    		<&axi_ad9081_core_tx 0 DEFRAMER_LINK0_TX>;
    
    		adi,tx-dacs {
    			#size-cells = <0>;
    			#address-cells = <1>;
    			adi,dac-frequency-hz = /bits/ 64 <6000000000>;
    
    			adi,main-data-paths {
    				#address-cells = <1>;
    				#size-cells = <0>;
    				adi,interpolation = <2>;
    
    				ad9081_dac0: dac@0 {
    					reg = <0>;
    					adi,crossbar-select = <&ad9081_tx_fddc_chan0>;
    					adi,nco-frequency-shift-hz = /bits/ 64 <100000000>; /* 100 MHz */
    				};
    
    				ad9081_dac1: dac@1 {
    					reg = <1>;
    					adi,crossbar-select = <&ad9081_tx_fddc_chan1>;
    					adi,nco-frequency-shift-hz = /bits/ 64 <100000000>; /* 100 MHz */
    				};
    			};
    
    			adi,channelizer-paths {
    				#address-cells = <1>;
    				#size-cells = <0>;
    				adi,interpolation = <1>;
    
    				ad9081_tx_fddc_chan0: channel@0 {
    					reg = <0>;
    					adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
    					adi,nco-frequency-shift-hz =  /bits/ 64 <0>;
    				};
    
    				ad9081_tx_fddc_chan1: channel@1 {
    					reg = <1>;
    					adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
    					adi,nco-frequency-shift-hz =  /bits/ 64 <0>;
    				};
    			};
    
    			adi,jesd-links {
    				#size-cells = <0>;
    				#address-cells = <1>;
    
    				ad9081_tx_jesd_l0: link@0 {
    					#address-cells = <1>;
    					#size-cells = <0>;
    					reg = <0>;
    					adi,logical-lane-mapping = /bits/ 8 <0 2 7 6 1 5 4 3>;
    					adi,link-mode = <17>;			/* JESD Quick Configuration Mode */
    					adi,subclass = <1>;			/* JESD SUBCLASS 0,1,2 */
    					adi,version = <2>;			/* JESD VERSION 0=204A,1=204B,2=204C */
    					adi,dual-link = <0>;			/* JESD Dual Link Mode */
    					adi,converters-per-device = <4>;	/* JESD M */
    					adi,octets-per-frame = <1>;		/* JESD F */
    					adi,frames-per-multiframe = <256>;	/* JESD K */
    					adi,converter-resolution = <16>;	/* JESD N */
    					adi,bits-per-sample = <16>;		/* JESD NP' */
    					adi,control-bits-per-sample = <0>;	/* JESD CS */
    					adi,lanes-per-device = <8>;		/* JESD L */
    					adi,samples-per-converter-per-frame = <1>; /* JESD S */
    					adi,high-density = <1>;			/* JESD HD */
    
    					adi,tpl-phase-adjust = <0x3b>;
    				};
    			};
    		};
    
    		adi,rx-adcs {
    			#size-cells = <0>;
    			#address-cells = <1>;
    			adi,adc-frequency-hz = /bits/ 64 <6000000000>;
    
    			adi,main-data-paths {
    				#address-cells = <1>;
    				#size-cells = <0>;
    
    				ad9081_adc0: adc@0 {
    					reg = <0>;
    					adi,decimation = <2>;
    					adi,nco-frequency-shift-hz =  /bits/ 64 <100000000>;
    					adi,nco-mixer-mode = <AD9081_ADC_NCO_VIF>;
    				};
    
    				ad9081_adc1: adc@1 {
    					reg = <1>;
    					adi,decimation = <2>;
    					adi,nco-frequency-shift-hz =  /bits/ 64 <100000000>;
    					adi,nco-mixer-mode = <AD9081_ADC_NCO_VIF>;
    				};
    			};
    
    			adi,channelizer-paths {
    				#address-cells = <1>;
    				#size-cells = <0>;
    
    				ad9081_rx_fddc_chan0: channel@0 {
    					reg = <0>;
    					adi,decimation = <1>;
    					adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
    					adi,nco-frequency-shift-hz =  /bits/ 64 <0>;
    				};
    
    				ad9081_rx_fddc_chan1: channel@1 {
    					reg = <1>;
    					adi,decimation = <1>;
    					adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
    					adi,nco-frequency-shift-hz =  /bits/ 64 <0>;
    				};
    			};
    
    			adi,jesd-links {
    				#size-cells = <0>;
    				#address-cells = <1>;
    
    				ad9081_rx_jesd_l0: link@0 {
    					reg = <0>;
    					adi,converter-select =
    					<&ad9081_rx_fddc_chan0 FDDC_I>, <&ad9081_rx_fddc_chan0 FDDC_Q>,
    					<&ad9081_rx_fddc_chan1 FDDC_I>, <&ad9081_rx_fddc_chan1 FDDC_Q>;
    
    					adi,logical-lane-mapping = /bits/ 8 <2 0 7 6 5 4 3 1>;
    					adi,link-mode = <18>;			/* JESD Quick Configuration Mode */
    					adi,subclass = <1>;			/* JESD SUBCLASS 0,1,2 */
    					adi,version = <2>;			/* JESD VERSION 0=204A,1=204B,2=204C */
    					adi,dual-link = <0>;			/* JESD Dual Link Mode */
    					adi,converters-per-device = <4>;	/* JESD M */
    					adi,octets-per-frame = <1>;		/* JESD F */
    					adi,frames-per-multiframe = <256>;	/* JESD K */
    					adi,converter-resolution = <16>;	/* JESD N */
    					adi,bits-per-sample = <16>;		/* JESD NP' */
    					adi,control-bits-per-sample = <0>;	/* JESD CS */
    					adi,lanes-per-device = <8>;		/* JESD L */
    					adi,samples-per-converter-per-frame = <1>; /* JESD S */
    					adi,high-density = <1>;			/* JESD HD */
    				};
    			};
    		};
    
    	};
    };

    I can confirm the new DAC rate through IIO, but I tried to send a CW tone with DDS (/DMA) and unfortunately still got nothing:

    It's perhaps a long shot, but I do suspect the TX/RX device clocks are too fast at 375MHz. I wonder if lowering them would maybe help, what are your thoughts? I found a configuration in another post for the vpk180 which shows the following:

    Link clock is still 375 MHz but device clocks are at 250MHz. How can I achieve this? I tried changing the clocks in the device tree but I wasn't sure which, there are multiple RX/TX core clocks. I also wonder if changes in the HDL design are needed to change those clocks, I wasn't able to find those configurations in the HDL design blocks.

    Let me know if any more info is needed. Thank your for continued support in the matter!

    OR1

  • Sorry to hear of the trouble again. 

    The 375MHz link clock is well within the acceptable range, and your configuration does not need a gearbox so the link clock and device clock are same. The other case with 250MHz of device clock that you referenced requires gearbox becuase NP=12, so that is not applicable to you. Refer to the following page for more details about gearbox: analogdevicesinc.github.io/.../fpga_internal.html

    So, we'll keep looking. Have you tried any other configuration that works?

    -YH

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.