Hi,
We have the following observation in the AD9081-FMCA-EBZ Board. Kindly, help us resolve this query.

- If we are supposed to maintain 50 ohms for DAC, won't there be impedance mismatch if we give 100 ohm termination for DAC in the simulation model?
- And if we are maintaining the traces in the board-file as 50 ohms for ADC, it will again bring a mismatch if we give 100 ohm termination for ADC in the simulation model.
For DAC: For ADC:

Also, we have seen that in the AD9988_AD9986(which is similar to AD9081 apart from the difference in bandwidth and other specs) Board-files available in the website, we have seen that TCM1-83X+ Balun has been used and the ADC differential traces in that case have been maintained for 100 ohm differential and for DAC it is maintained for 50 ohm differential.
Edit Notes
The subject title has been changed[edited by: Utstech at 5:17 AM (GMT -5) on 7 Mar 2025]