Hello there,
AD9082 user guide 1578 recommends use of Buck ADP5056 and ADP7158, ADP1765 LDOs. I'm looking for possible alternative for AD9082 power supply.
ADP7158
Recommended for New Designs
The ADP7158 is a linear regulator that operates from 2.3 V to 5.5 V and provides up to 2 A of output current. Using an advanced proprietary architecture...
ADP7158 on Analog.com
ADP1765
Recommended for New Designs
The ADP1765 is a low noise, low dropout (LDO) linear regulator. It is designed to operate from a single input supply with an input voltage as low as 1...
Datasheet
ADP1765 on Analog.com
Hello there,
AD9082 user guide 1578 recommends use of Buck ADP5056 and ADP7158, ADP1765 LDOs. I'm looking for possible alternative for AD9082 power supply.
Could you tell us the reason why you are looking for alternatives?
Could you tell us the reason why you are looking for alternatives?
The card i'm working on has size constraints.
If the size matters, the ADP5056 based solution would be a better option. And you may have to keep those LDOs (ADP7158, ADP1765) for better noise performance.
AD9082-FMCA EVB uses two micro modules of LTM4616 and LTM4644, while FMCB EVB uses ADP5056. Please take a look at the schematics of the FMCB EVB as a starting point (https://www.analog.com/media/en/technical-documentation/eval-board-schematic/eval-ad9988-ad9986-schematic.pdf), There are large current sensing resistors for 1V inputs to LDOs in FMCB EVB, which you can remove, and overall area of ADP5056 based solution woudl be rather small.

Hope this helps and let us know if you need further clarificaiton.
thank you so much !