I am using VCU118 board + AD9082 with setup as shown in link https://wiki.analog.com/resources/eval/user-guides/ad9081_fmca_ebz/quickstart/microblaze but with AD9082 board.
Using HMC to generate 125 MHz as CLK and Feeding 4.4GHz (5dBm) to EXT_CLK input of AD9082 and bypassing the PLL, capacitors C4D & C6D are mounted and C3D and C5D are un-mounted.
I am able to read and write into ADC9082 & HMC registers.
The aim is to energize the ADC of AD9082 @ 4.4GHz, and transmit the sampled data over JESD204C 64b/66b.
In order to do so, The following registers are configured as per UG-1578.
| SNO | ADDR | DESC | B7 | B6 | B5 | B4 | B3 | B2 | B1 | B0 | VAL | DESC |
| 1 | 0x001A | JTX_PAGE | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0x01 | EN LINK 0 ONLY |
| 2 | 0x0710 | FORCE_LINK_RESET_REG | 0 | 0 | 0 | 1 | 0 | 0 | 0 | 1 | 0x11 | FORCE RESET SELECTED JTX LINK |
| 3 | 0x0600 | JTX_CORE_0_CONV0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0x00 | |
| 4 | 0x0601 | JTX_CORE_0_CONV1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0x01 | |
| 5 | 0x0750 | PWR_DN | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0x00 | POWER UP Serializer |
| 6 | 0xEFFF | DELAY | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0x00 | DELAY |
| 7 | 0x061B | JTX_CORE2_LANE0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0x00 | FORCE DOWN LANE 0 |
| 8 | 0x061C | JTX_CORE2_LANE1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0x01 | FORCE DOWN LANE 1 |
| 9 | 0x061D | JTX_CORE2_LANE2 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 0x02 | FORCE DOWN LANE 2 |
| 10 | 0x061E | JTX_CORE2_LANE3 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 1 | 0x03 | FORCE DOWN LANE 3 |
| 11 | 0x061F | JTX_CORE2_LANE4 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 0 | 0x04 | FORCE DOWN LANE 4 |
| 12 | 0x0620 | JTX_CORE2_LANE5 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 1 | 0x05 | FORCE DOWN LANE 5 |
| 13 | 0x0621 | JTX_CORE2_LANE6 | 0 | 0 | 0 | 0 | 0 | 1 | 1 | 0 | 0x06 | FORCE DOWN LANE 6 |
| 14 | 0x0622 | JTX_CORE2_LANE7 | 0 | 0 | 0 | 0 | 0 | 1 | 1 | 1 | 0x07 | FORCE DOWN LANE 7 |
| 15 | 0xEFFF | DELAY | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0x00 | DELAY |
| 16 | 0x0782 | EN_DRVSLICEOFFSET | 0 | 0 | 0 | 0 | 1 | 1 | 1 | 1 | 0x0F | EN_DRVSLICEOFFSET |
| 17 | 0x0752 | JTX_SWING | 0 | 0 | 0 | 1 | 0 | 0 | 0 | 1 | 0x11 | 0.85*SVDD1, Default |
| 18 | 0x0763 | PRE_TAP_LEVEL_CH0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0x00 | 0dB, default |
| 19 | 0x075A | POST_TAP_LEVEL1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0x00 | 0dB, default |
| 20 | 0x0789 | MAIN_DATA_INV | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0x00 | JTX Invert = normal, default |
| 21 | 0x0773 | RSTB | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 0xFF | Reset Digital Logic |
| 22 | 0xEFFF | DELAY | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0x00 | DELAY |
| 23 | 0x0773 | RSTB | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0x00 | Reset Digital Logic |
| 24 | 0xEFFF | DELAY | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0x00 | DELAY |
| 25 | 0x0773 | RSTB | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 0xFF | Reset Digital Logic |
| 26 | 0xEFFF | DELAY | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0x00 | DELAY |
| 27 | 0x0710 | FORCE_LINK_RESET_REG | 0 | 0 | 0 | 1 | 0 | 0 | 0 | 1 | 0x11 | FORCE RESET SELECTED JTX LINK |
| 28 | 0x001A | JTX_PAGE | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0x01 | EN LINK 0 ONLY |
| 29 | 0x0721 | PLL_ENABLE_CTRL | 0 | 0 | 1 | 0 | 0 | 0 | 0 | 0 | 0x20 | LCPLL_JTX_PLL_BYPASS_LOCK |
| 30 | 0x0712 | K_EMB_QC_OVERRIDE | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0x01 | k_emb qc values override in qc mode |
| 31 | 0x063D | JTX_L0_3 | 1 | 0 | 0 | 0 | 0 | 1 | 1 | 1 | 0x87 | Scramble En |
| 32 | 0x063E | JTX_F_CFG | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0x00 | 1 Octate |
| 33 | 0x063F | JTX_K_CFG | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 0xFF | K=256 |
| 34 | 0x0640 | JTX_M_CFG | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0x01 | M= 2 |
| 35 | 0x0641 | JTX_CS_CFG | 0 | 0 | 0 | 0 | 1 | 1 | 1 | 1 | 0x0F | Default, no Of CS = 0, 16 bit resolution |
| 36 | 0x0642 | JTX_SUBCLASSV_CFG | 0 | 0 | 1 | 0 | 1 | 0 | 1 | 1 | 0x2B | Sub-Class 1, ADC 12 bits per sample |
| 37 | 0x0643 | JTX_JESDV_CFG | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0x01 | S = no of samples per frame per cycle = 1 |
| 38 | 0x0636 | JTX_TPL_6 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0x00 | MASK for sub-Class 1 |
| 39 | 0x0644 | JTX_HD_CFG | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0x80 | HD bit |
| 40 | 0x0773 | RSTB | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 0xFF | Reset Digital Logic |
| 41 | 0xEFFF | DELAY | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0x00 | DELAY |
| 42 | 0x0773 | RSTB | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0x00 | Reset Digital Logic |
| 43 | 0xEFFF | DELAY | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0x00 | DELAY |
| 44 | 0x0773 | RSTB | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 0xFF | Reset Digital Logic |
| 45 | 0xEFFF | DELAY | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0x00 | DELAY |
| 46 | 0x0773 | RSTB | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 0xFF | |
| 47 | 0x0668 | JTX_DL_204C_1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0x00 | Default |
| 48 | 0x0611 | JTX_CORE_1 | 0 | 0 | 0 | 1 | 0 | 0 | 0 | 0 | 0x10 | |
| 49 | 0x062E | JTX_CORE_13 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0x01 | |
| 50 | 0x0670 | JTX_PHY_IFX_0_LANEn | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0x00 | |
| 51 | 0x0671 | JTX_PHY_IFX_1_LANEn | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0x00 | |
| 52 | 0x0672 | JTX_PHY_IFX_2_LANEn | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0x00 | Async False |
| 53 | 0x0673 | JTX_PHY_IFX_3_LANEn | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0x00 | Async Mode |
| 54 | 0x0674 | JTX_PHY_IFX_4_LANEn | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0x00 | Selects JESD204B/C parallel data processing width. 0 = 66 bits (204C) |
| 55 | 0x0675 | JTX_PHY_IFX_5_LANEn | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0x00 | |
| 56 | 0x0676 | JTX_PHY_IFX_6_LANEn | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0x00 | |
| 57 | 0x0677 | JTX_PHY_IFX_7_LANEn | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0x00 |
| 58 | 0x0630 | JTX_TPL_0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0x00 | |
| 59 | 0x070A | JTX_SER_BIT_FIELD | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0x01 | Lane rate > 16Gbps, may be checked |
| 60 | 0x0762 | PARDATAMODE_SER | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0x00 | FORCE RESET SELECTED JTX LINK |
| 61 | 0x0797 | SYNCA_CTRL | 0 | 0 | 0 | 0 | 1 | 0 | 0 | 1 | 0x09 | One shot sync |
| 62 | 0x0798 | SYNCB_CTRL | 0 | 0 | 0 | 0 | 1 | 0 | 0 | 1 | 0x09 | |
| 63 | 0x0706 | JTX_SER_CLK_INVERT | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0x00 | |
| 64 | 0x0727 | LCPLL_REF_CLK_DIV1_REG | 0 | 0 | 0 | 1 | 0 | 0 | 0 | 1 | 0x11 | |
| 65 | 0x0717 | DVM_LCPLL_RC_RX | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 0x02 | |
| 66 | 0x0710 | FORCE_LINK_RESET_REG | 0 | 0 | 0 | 1 | 0 | 0 | 0 | 1 | 0x11 | |
| 67 | 0x00B8 | SYSREF_MODE | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 0x02 |
During setting it is observed that when setting reg 0x061B to 0x0622 the value read back is 0x80, 0x81...0x87 not 0x00, 0x01, .... 0x07.
which implies that the Lane is not up. JTX_LANE0_PD_STATUS bit 7 is high, implying Lane is power down. Requested to provide possible reason Lane is not UP and also share the correct setting to be carried out.
The following values are shared for device info:
| REG | DATA |
| 0x701 | 0x80 |
| 0x722 | 0x1 |
| 0x713 | 0x0 |
| 0x0 | 0x18 |
| 0x3 | 0xF |
| 0x4 | 0x82 |
| 0x5 | 0x90 |
| 0x6 | 0x23 |
| 0xB | 0x1 |
| 0xC | 0x56 |
| 0xD | 0x4 |
| 0x10 | 0x0 |
| 0x11 | 0x0 |
| 0x12 | 0x0 |
| 0x13 | 0x0 |
| 0x210 | 0x3F |
| 0x211 | 0xF |
| 0x212 | 0x3F |
| 0x213 | 0x3F |
| 0x2107 | 0x0 |
| 0x2108 | 0x0 |
| 0x210B | 0x0 |
| 0x210C | 0x0 |
It is also observed that the temperature registers 0x2107, 0x2108, 0x210B & 0x210C are read as zeros.
Hello,
With regard to description "Using HMC to generate 125 MHz as CLK and Feeding 4.4GHz (5dBm) to EXT_CLK input of AD9082 and bypassing the PLL, capacitors C4D & C6D are mounted and C3D and C5D are un-mounted"............................it would appear that the "SERDES REFCLK" is either not being provided and/or is not locked to the 4.4 GHz external clock signal. For a successful JESD204 link to occur.............both the clock provided to the AD9082 (i.e. EXT_CLK in your case) as well as the reference clock provided to FPGA (which is used by its SERDES PLL) must be phase locked to ensure that the lane rates are at exactly the same frequency and are phase aligned (i.e. no drift in phase). Note that when one uses the HMC7044 to provide both the clock to the AD9082 as well as the ref clock (via FMC connector pins).................these two signals being derived off the same HMC PLL2/VCO are considered locked.
With regard to your settings...................the SPI writes that occur should be based on the AD9082 API which generates all the necessary SPI writes to configure the device (as well as exact order in which they must occur). It is unclear from your description on whether the AD9082 SPI configuration file is based on our API.
Note that our ACE based GUI provides a means of configuring the AD9082 from a high level when interfacing to our ADS9-V2 FPGA capture board. One can inspect the "SPI writes" used to configure the device via downloading the log file. Assuming that you have a ADS9-V2 board..............perhaps it would be best to use this 1st to verify that your desired configuration does work before moving to implement on another FPGA platform. Note that the Tx (and Rx) ref clock corresponds to the clock frequency that is required by the FPGA to that its clocks are phase aligned with the AD9082. In the case of applying an external ref clock to the AD9082 FMCA EVB...............one must also apply an external reference clock to the FPGA via another RF generator that is phase locked (via 10 MHz REF OUT/IN connection on back of instrument with master/slave relationship).
Regards
Hello,
With regard to description "Using HMC to generate 125 MHz as CLK and Feeding 4.4GHz (5dBm) to EXT_CLK input of AD9082 and bypassing the PLL, capacitors C4D & C6D are mounted and C3D and C5D are un-mounted"............................it would appear that the "SERDES REFCLK" is either not being provided and/or is not locked to the 4.4 GHz external clock signal. For a successful JESD204 link to occur.............both the clock provided to the AD9082 (i.e. EXT_CLK in your case) as well as the reference clock provided to FPGA (which is used by its SERDES PLL) must be phase locked to ensure that the lane rates are at exactly the same frequency and are phase aligned (i.e. no drift in phase). Note that when one uses the HMC7044 to provide both the clock to the AD9082 as well as the ref clock (via FMC connector pins).................these two signals being derived off the same HMC PLL2/VCO are considered locked.
With regard to your settings...................the SPI writes that occur should be based on the AD9082 API which generates all the necessary SPI writes to configure the device (as well as exact order in which they must occur). It is unclear from your description on whether the AD9082 SPI configuration file is based on our API.
Note that our ACE based GUI provides a means of configuring the AD9082 from a high level when interfacing to our ADS9-V2 FPGA capture board. One can inspect the "SPI writes" used to configure the device via downloading the log file. Assuming that you have a ADS9-V2 board..............perhaps it would be best to use this 1st to verify that your desired configuration does work before moving to implement on another FPGA platform. Note that the Tx (and Rx) ref clock corresponds to the clock frequency that is required by the FPGA to that its clocks are phase aligned with the AD9082. In the case of applying an external ref clock to the AD9082 FMCA EVB...............one must also apply an external reference clock to the FPGA via another RF generator that is phase locked (via 10 MHz REF OUT/IN connection on back of instrument with master/slave relationship).
Regards
Hello,
I will let my software colleagues who support the example code associated with VCU118. The earlier point about using ext clock is still relevant. As such............I suggest that you use HMC7044 as your clocking solution (C5D, C3D populated) and try one of the proven design examples to demonstrate that you have working software and set-up. Once this has been demonstrated...........then create your own use case example (still using the HMC7044 as clock source) and start debug process.
Regards

Thank you for the reply,
1) I will try phase locking both the clocks and check if lane gets up.
2) I have tried running the hardware with the highlighted files, as per procedure of https://wiki.analog.com/resources/eval/user-guides/ad9081_fmca_ebz/quickstart/microblaze
It is observed that for my AD9082 daughter board when it boots, in "dmesg" it said "ad9082 spi0.0: Unrecognized CHIP_ID 0x9082"
I think those files are compiled for only AD9081 but not for AD9082,
When booting through those files, IIO scope shows only HMC but not AD9082.
If possible please share compiled binaries for AD9082 with VCU118.
3) I don't have ADS9-V2 FPGA capture board at present and ACE software doesn't update its memory map. I have raised a support request for the same in https://ez.analog.com/wide-band-rf-transceivers/mixed-signal-front-ends-mxfe/f/q-a/558109/memory-map-not-updating-after-clicking-apply-of-quick-configuration-no-harware.
4) It is also observed that the temperature registers 0x2107, 0x2108, 0x210B & 0x210C are read as zeros, possible reasons for such behavior.
The only thing possible to test for me in current setup is with option 1, I shall try it and get back.
Regards,
Faiz Ahmed.