Can I use AD8372 with the input and output in a single ended circuit?

Is there an application circuit of AD8372 for single ended (both input and output) case?

Parents
  • 0
    •  Analog Employees 
    on Jul 30, 2018 6:06 PM

    We have not developed or tested an application circuit for single-ended operation. I would suggest ac-coupling INC1 to ground. Alternatively, you could try putting a 75 ohm resistor in series with the ac-coupling cap on INC1

    On the output put the same load on the unused output (i.e. a dummy load) as you have on the used output.

Reply
  • 0
    •  Analog Employees 
    on Jul 30, 2018 6:06 PM

    We have not developed or tested an application circuit for single-ended operation. I would suggest ac-coupling INC1 to ground. Alternatively, you could try putting a 75 ohm resistor in series with the ac-coupling cap on INC1

    On the output put the same load on the unused output (i.e. a dummy load) as you have on the used output.

Children
No Data