Post Go back to editing

ADF4355-2-2 auto bleed current

The windows application auto calculates the negative bleed current, even if FRAC1 and FRAC2 are not 0, but from the ADF4355-2 Rev C page 25, :

"Use negative bleed only when operating in fractional-N mode,
that is, FRAC1 = FRAC2 = 0. Do not use negative bleed for f PFD
greater than 100 MHz."

Which is correct?

(Is it possible to get the source code for the Windows Application)