HMC641ALC4 Maximum input power

Hello,

I have a question about maximum input power at Hot Switching of HMC641ALC4. As for HMC641ALP4E, the maximum input power at Hot Switching is defined in the ABSOLUTE MAXIMUM RATING of the datasheet. On the other hand, as for HMC641ALC4, it is not defined in the datasheet. Is the spec of the maximum input power at Hot Switching of HMC641ALC4 same as HMC641ALP4E?

Best regards,

Akira

Parents
  • Hi,

    HMC641ALC4 and HMC641ALP4E use same die in different package types so they have same power handling performance.

    We had updated HMC641ALP4E datasheet from legacy HMC format to ADI format and added power handling ratings for hot switching operation. The same power handling ratings are valid also for HMC641ALC4.

    Best.

Reply
  • Hi,

    HMC641ALC4 and HMC641ALP4E use same die in different package types so they have same power handling performance.

    We had updated HMC641ALP4E datasheet from legacy HMC format to ADI format and added power handling ratings for hot switching operation. The same power handling ratings are valid also for HMC641ALC4.

    Best.

Children
No Data