Post Go back to editing

HMC773ALC3B

Thread Summary

The user inquired about the HMC773ALC3B mixer's performance as an upconverter with IF at 4.5 GHz, LO from 9.5 to 10.5 GHz, and RF from 5 to 6 GHz (LOWER SIDEBAND). The final answer stated that data for these frequencies is not available, and recommended testing with an evaluation board, noting that performance below the specified 6 GHz RF is not guaranteed.
AI Generated Content

Hello,

Do you have any data about the HMC773ALC3B behaviour working as upconverter with the following frequencies?

IF= 4.5Ghz

LO= 9.5Ghz to 10.5 GHz

RF= 5Ghz to 6GHz (LOWER SIDEBAND)

Even if according to the data sheet, min RF is 6Ghz, there is no rolloff on the conversion loss at 6 GHz so it looks like the mixer could work below this frequency.