I'm looking to use the ADL5570 down to 2200MHz. It's a CW application. Sounds doable, but wanted to check. Would I have to change the output match?
Thanks,
Tim
ADL5570
Obsolete
The ADL5570 is a high linearity 2.3 GHz to 2.4 GHz power amplifier designed for WiMAX terminals using TDD operation at a duty cycle of 31%. With a gain...
Datasheet
ADL5570 on Analog.com
I'm looking to use the ADL5570 down to 2200MHz. It's a CW application. Sounds doable, but wanted to check. Would I have to change the output match?
Thanks,
Tim
CW application at 2200MHz will not work for the ADL5570. CW signal can overheat the part. The part is quite sensitive and is specifically tuned for a 100MHz BW operation. (2300MHz to 2400MHz)