Is ADL5535 designed for a specific output power?

I called in to ADI's tech support asking why I was getting less OIP3 than what is stated in the specification section in the datasheet and was pointed to figure 7 on page 8 showing OIP3 versus output power.  I see there a significant spike in OIP3 at Pout=3dBm.  Is there a specific reason why OIP3 is best at 3dBm?  Was it designed to be this way?

  • 0
    •  Analog Employees 
    on Jun 2, 2010 3:42 PM over 10 years ago

    The ADL5535 has a harmonic cancellation circuit which improves OIP3. The draw back to this approach is optimization is limited to a particular frequency and not the entire bandwidth of the amplifier.  It is expected that someone using the ADL5535 would operate around 0 dBm output power. This would allow for large crestfactor swings WCDMA type modulated signals and not drive the amplifier beyond its 1 dB compression point.

  • 0
    •  Analog Employees 
    on Aug 2, 2018 4:11 PM over 2 years ago
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin