ADL5519

I am looking at a wide dynamic range RF detector (~60dB) to operate in the 0.5 - 2.2GHz range. This is for various signal types up to W-CDMA PAR and bandwidth, with the desire to measure the peak independant of the signal modulation. There seems to be two options, neither of which is quite right and so I would like some help on the best choice. The ADL5502 performs RMS and peak measurements, but with limited dynamic range and I suspect not enough bandwidth while the ADL5519 has the dynamic range and bandwidth but not the peak capabilities.  I have an evaluation board for the ADL5519 and am trying to make a descrete peak detector essentially like the 5502 but to operate at lower frequency on the (log) baseband modulation from the ADL5513 video output.

Any help appreciated

Parents Reply Children
No Data