Post Go back to editing

RF equipment for ADXL193 on moving animal

Dear colleagues.

WE are normally using SD card logged GPS time synced data but are currently working on a project with multiple channel input to a powerlab 16/35 and collected via labchart.

We're looking for suggestions on RF equipment to use with this setup and a 3-axis accelerometer constructed from 3 kevlar embedded ADXL193's and attached to the horses' leg where the transmitter and battery should be fairly lightweight sturdy and able to handle 250g accelerations attached to the horses' leg. Data should be transmitted at 2000Hz.

All suggestions are welcome and greatly appreciated!

/Emil Olsen

DVM, clinical biomechanist, UK.

Parents Reply Children
No Data