Hi,
I have a yagi antenna and I want to evaluate the radiation pattern by connecting the antenna to the AD8314 eval board and monitoring the signal strength on an oscilloscope. The antenna characteristics are:
Frequency Range: 2400-2500 GHz
Gain: 7.5+0.5dBi
VSWR: 1.8:1 max
Impedance: 50
Polarization: Linear vertical
HPBW/vertical: 60
Front to back ratio: 15dB
Connector: Re-SMA standard
I would like to know the simplest way to connect this antenna to the eval board and where to get the components.
thank you,
Wilburn