- Hello.
I've ADRF6704 the evaluation board circuit embedded in my project.
I installed this software ADRF6x0x_customer_6p1p0.
I use the EZ-USB-Interface software download ADRF6x0x_6p1p0.hex.
But I encountered a problem.
My system is WIN7.
Under “Computer Management \ Device
Manager \ Universal Serial
Bus Controller|”
can not display the
correct hardware drivers,
but is CypressEZ-USB FX2LP-EEPROM missing.
But "ADRF6x0x eval
board connected" is displayed in “Anakig Devices ADRF6x0x Customer Evaluation Software v6.1.0-ADRF6704
TxMod 2500-2900MHz” interface .
May I ask what is the reason?
Since I design careless,
The 68013A's pins for PA2 --- DATA,
PA1--CLK.,
I want to be able to get the firmware source codes
To modify the control program, this does not change the hardware circuit.
My project PDF file is attached.
I would appreciate if help soon.