The ADRF6704 Debug Advisory and get help

  1. Hello.

    I've ADRF6704 the evaluation board circuit  embedded in my project.

I installed this software ADRF6x0x_customer_6p1p0.



I use the EZ-USB-Interface software download ADRF6x0x_6p1p0.hex.



But I encountered a problem.

My system is WIN7.

 

Under “Computer Management \ Device
Manager
\ Universal Serial
Bus Controller|”

can not display the
correct
hardware drivers,

but is CypressEZ-USB FX2LP-EEPROM missing.

 

But "ADRF6x0x eval
board connected" is displayed
inAnakig Devices ADRF6x0x Customer Evaluation Software v6.1.0-ADRF6704
TxMod 2500-2900MHz”
interface .



May I ask what is the reason?

 

Since I design careless,

The 68013A's pins for PA2 --- DATA,
PA1--CLK.,

I want to be able to get the firmware source codes

To modify the control program, this does not change the hardware circuit.

My project PDF file  is attached.




I would appreciate if help soon.

RF_QM_Tx.pdf
  • 0
    •  Analog Employees 
    on Mar 11, 2013 10:45 PM

    For the circuit to program correctly, the EEPROM must be programmed with the correct sequence in its first few memory registers. The first code in reg 0x00 should be 0xc0, which will tell the system that the microcode on the uprocessor on the 68013 will be downloaded from the pc itself as part of the software execution. The next four registers will contain the vendor ID and product ID for the evaluation board. Note that these are vendor specific and should not be used on a customers final product. The first five registers are therefore as follows;

    "0xc0";

    "0x56"

    "0x04"

    "0x50"

    "0x70"

    If you're going to go down this road of adding the Cypress USB chip and EEPROM to your design, you will really need to dig into the Cypress documentation, we're really not prepared to help you with this.  Unfortunately, we're not in the habit of giving away the source code to our eval boards and if we do, we're not going to be supporting debugging it or adapting it for your specific application. Let me know if there is anything more I can do to help you.

  • I encountered a strange problem:

    Plug in any board with usb 68013A,

    No download firmware, debug software for ADRF670 opens,

    The status bar of debugging software always shows the following "ADRF6x0x eval board connected".

    Why is ti???

     

  • Supplement:

    I've debugged the the ADF 4360 series devices and ADRF435X series, AD9518 family of devices。

  • 0
    •  Analog Employees 
    on Aug 2, 2018 4:48 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin