Hi,
Just wondering if the ADL5320or similar SOT-89 packaged part might work down to 145Mhz?
I need the following specs for an amplifier:
Fout = 145MHz
P1dB ~ 20dBm
Gain ~ 12dB
Thanks,
Rev.
Hi Rev.,
Internal circuitry prevents the ADL5320 from operating below 400 MHz.
I suggest looking at the ADL5601, ADL5602, ADL5535 and ADL5536. the ADL5601 and ADL5535 are 15 dB gain blocks and will operate at 145 MHz. THe ADL5602 and ADL5536 are similar devices and have 20 dB of gain.
The operating frequency range for the ADL5601/02 is: 50 MHz to 4 Ghz. For the ADL5535 and ADL5536 the frequency range is: 20 MHz to 1 GHz.
Hi Rev.,
Internal circuitry prevents the ADL5320 from operating below 400 MHz.
I suggest looking at the ADL5601, ADL5602, ADL5535 and ADL5536. the ADL5601 and ADL5535 are 15 dB gain blocks and will operate at 145 MHz. THe ADL5602 and ADL5536 are similar devices and have 20 dB of gain.
The operating frequency range for the ADL5601/02 is: 50 MHz to 4 Ghz. For the ADL5535 and ADL5536 the frequency range is: 20 MHz to 1 GHz.