Post Go back to editing

ADF4156 Design Issue at 1911.642 MHz

Hello!

I've been using ADF4156 to design Local Oscillators at frequencies in the range of 5 to 6 GHz.

I use ADISimPLL and Fraction N software for the design.

I haven't faced any difficulties in the LO design at the above mentioned frequencies; but, i am facing difficulties in designing a LO at 1911.642 MHz.

The LO worked fine initially, but, strangely enough, it stopped working afterwards.

The charge pump output voltage is at 0.4V to 0.5V no matter what register configuration i use.

Further, the PLL chip gives out 5V at the charge pump out if i only enable the charge pump supply.

I've also designed a test PCB of ADF4156, but the PLL chip responds the same way.

Kindly help me in resolving this issue.

Am i programming the chip wrong?

It should not be the case as the LO was working initially.

An example for designing the LO at 1911.642MHz using Fraction N software and ADISimPLL would be highly helpful.

Thanking you in anticipation.

With best regards,

Humayun Zahid

Parents
  • Hi Brigid!

    The question was originally posted by me.

    A channel spacing of 2 KHz was used and Z-Com V674ME08 VCO was used.

    The design issue has been resolved; the problem was with the prescaler value; i was using 8/9 instead of 4/5.

    I use Windows 7, and the AD's Fractional N software wasn't showing an error on using the 8/9 prescaler below 3 GHz.

    But, strangely enough, the LO was working previously when i used the 8/9 prescaler. 

    So, this question still remains un-answered as to how it was working by using a prescaler of 8/9 (provided all the other settings were same).

    thanks for your support.

    with best regards,

    Humayun Zahid

Reply
  • Hi Brigid!

    The question was originally posted by me.

    A channel spacing of 2 KHz was used and Z-Com V674ME08 VCO was used.

    The design issue has been resolved; the problem was with the prescaler value; i was using 8/9 instead of 4/5.

    I use Windows 7, and the AD's Fractional N software wasn't showing an error on using the 8/9 prescaler below 3 GHz.

    But, strangely enough, the LO was working previously when i used the 8/9 prescaler. 

    So, this question still remains un-answered as to how it was working by using a prescaler of 8/9 (provided all the other settings were same).

    thanks for your support.

    with best regards,

    Humayun Zahid

Children
No Data