Question 1. The Power Amplifier ADL5324 Evaluation Board's default frequency is 2110 MHz - 2170 MHz. But I want it to work at frequency of 3100 MHz - 3400 MHz. Is it possible to simulate the matching network in ADS? Like the picture shows.
The simulation result seems different from the datasheet. Or maybe I could only modify the component on the board directly?
Question 2. I also want the LNA ADL5523 evaluation board to work at frequency of 3100 MHz to 3400 MHz. As it is a LNA, we want to tune it for optimal noise figure. But it seems impossible to simulate it in ADS because I looked the SNP file and there is no data about Noise Figure, Fmin, GAMMA OPT. Could anyone tell me how to design the matching network?