Post Go back to editing

How to design the matching network of ADL5324 and ADL5523

Hello!

I am trying to design the tuning the ADL5324 and ADL5523, here is my problem.

Question 1. The Power Amplifier ADL5324 Evaluation Board's default frequency is 2110 MHz - 2170 MHz. But I want it to work at frequency of 3100 MHz - 3400 MHz. Is it possible to simulate the matching network in ADS?  Like the picture shows.

The simulation result seems different from the datasheet. Or maybe I could only modify the component on the board directly?

Question 2. I also want the LNA ADL5523 evaluation board to work at frequency of 3100 MHz to 3400 MHz. As it is a LNA, we want to tune it for optimal noise figure.  But it seems impossible to simulate it in ADS because I looked the SNP file and there is no data about Noise Figure, Fmin, GAMMA OPT. Could anyone tell me how to design the matching network?

Any advice would be apprciate.

Thank you!

Chris

Parents
  • Hi Chris,

                    I would build simulation #2. This is based on my experience witht the error in the model. The S-Parameters posted in the datasheet are a subset of the S-Parameters from the S2P file posted on the web.

    The evaluation board material is IS410 and hasa dieelctric of 4.66. It looks like you are using 3.66. This could explain for some of the descrepancy.

Reply
  • Hi Chris,

                    I would build simulation #2. This is based on my experience witht the error in the model. The S-Parameters posted in the datasheet are a subset of the S-Parameters from the S2P file posted on the web.

    The evaluation board material is IS410 and hasa dieelctric of 4.66. It looks like you are using 3.66. This could explain for some of the descrepancy.

Children
No Data