Is HMC1015 only available in die? Are there any plans to offer it in a plastic surface-mount package?
HMC1015
Obsolete
The HMC1015 is a general purpose triple balanced mixer chip that can be used as a frequency converter with 16 to 22 GHz at the IF port and 26 to 32 GHz...
HMC1015 on Analog.com
Is HMC1015 only available in die? Are there any plans to offer it in a plastic surface-mount package?
The HMC1015 is not only available in die form, but in a LC3 package. The HMC1043LC3 utilizes the same die that is used as the HMC1015. The HMC1043LC3 utilizes a 3 x 3 mm QFN Ceramic High Frequency SMT Package that does not degrade the performance from the die environment to the package environment.