Post Go back to editing

HMC363S8G eval board noise at Low Frequency

Hi,

We are using eval board for the HMC363S8G and have some noise issues at lower frequencies.  The performance is good at input frequencies above 100 MHz, but when I lower my input frequency to 30 MHz (3.75MHZ output) I start to see spurs above the noise floor at various frequencies (11.25MHz, 18.75MHZ, and 26.5MHz) these are not expected.  My fundamental is -40dB.  Input level is at 4dBm.   Further, when I decrease my input frequency to 16MHz, I see no output spectrum other than white noise.

Can you help explain what I am doing wrong?

Parents
  • The "spurs" are indicative that the device is having difficulties. Although the datasheet indicates that it'll work down to DC this is a bit misleading - "close to DC"  would be more accurate. As one of our older parts, unfortunately it was only characterized to the "typical" minimum frequency of 200MHz listed in "Electrical Specification" table on page 1 of the datasheet. Below 200MHz the input and output return loss degrade sharply (IRL is ~ -7.5dB at 200MHz); to over come this the input power must be increased as indicated in the input sensitivity plots. Although the plots appear to go to DC, they really only go to 200MHz. Below 100MHz a square wave is required, the higher the slew rate the better and be sure that the DC blocking caps are sized appropriately for the frequency. We've seen some improvement in the input sensitivity at low frequencies by using ATC 530L or 550L broadband caps. Lastly try increasing the input power to 8-10dBm.

Reply
  • The "spurs" are indicative that the device is having difficulties. Although the datasheet indicates that it'll work down to DC this is a bit misleading - "close to DC"  would be more accurate. As one of our older parts, unfortunately it was only characterized to the "typical" minimum frequency of 200MHz listed in "Electrical Specification" table on page 1 of the datasheet. Below 200MHz the input and output return loss degrade sharply (IRL is ~ -7.5dB at 200MHz); to over come this the input power must be increased as indicated in the input sensitivity plots. Although the plots appear to go to DC, they really only go to 200MHz. Below 100MHz a square wave is required, the higher the slew rate the better and be sure that the DC blocking caps are sized appropriately for the frequency. We've seen some improvement in the input sensitivity at low frequencies by using ATC 530L or 550L broadband caps. Lastly try increasing the input power to 8-10dBm.

Children
No Data