Post Go back to editing

HMC241

Hello,

If ports RF1, RF2, RF3, or RF4 on the HMC241 are not connected to any circuitry, can the

non-connected port be left floating or is a DC blocking capacitor to gnd or VCC required to be connected to the unused port?

Best Regards.

Parents
  • FormerMember
    FormerMember
on Mar 18, 2015 2:26 PM
0

Hi,

The pins designated NC (Not Connected) are not internally connected to the die. It is not necessary to connect NC pins to any voltage, they can be left floating. However, the connection of NC pins to ground prevents noise injection from these pins, which may most probably distort RF and digital signals. We recommend to connect NC pins to ground.

Best.

Reply
  • FormerMember
    FormerMember
on Mar 18, 2015 2:26 PM
0

Hi,

The pins designated NC (Not Connected) are not internally connected to the die. It is not necessary to connect NC pins to any voltage, they can be left floating. However, the connection of NC pins to ground prevents noise injection from these pins, which may most probably distort RF and digital signals. We recommend to connect NC pins to ground.

Best.

Children
No Data