Post Go back to editing

HMC241

Hello,

If ports RF1, RF2, RF3, or RF4 on the HMC241 are not connected to any circuitry, can the

non-connected port be left floating or is a DC blocking capacitor to gnd or VCC required to be connected to the unused port?

Best Regards.

Parents
  • FormerMember
    FormerMember
on Jan 30, 2015 8:00 AM
0

Hi,

HMC241's RF ports are DC coupled with ~Vdd. Floating the unused RF ports would change the part performance slightly. We recommend terminating unused RF ports with 50 Ohm resistors to Vdd (DC blocking capacitor is not required but Vdd should be decoupled properly) or GND (DC blocking capacitor is required).

Regards

Reply
  • FormerMember
    FormerMember
on Jan 30, 2015 8:00 AM
0

Hi,

HMC241's RF ports are DC coupled with ~Vdd. Floating the unused RF ports would change the part performance slightly. We recommend terminating unused RF ports with 50 Ohm resistors to Vdd (DC blocking capacitor is not required but Vdd should be decoupled properly) or GND (DC blocking capacitor is required).

Regards

Children
No Data