We are trying to use the ADIismLINK Host Application with the EVAL-ADF70XXMBZ2 mother board and ADF7012DBZ Daughter board for use in a senior design project. When trying to configure the boards using the ADIismLINK v2 Host Application, the device type does not have an option to select the ADF7012 transmitter. The only selectable options are ADF7020, ADF7020-1, ADF7021, or ADF7025. How can we configure the boards with only these options available?