Post Go back to editing

Help with AD8302

Hi, I need to measure phase and magnitude of a signal against a reference in my project. Reading the datasheet, It seems that AD8302 evaluation board might be used for this.

I have a couple of questions that I wonder if someone can help though:

1) Both the input signal and reference are DC coupled square wave. The input signal is voltage output from a photodetector, and the reference is a output signal from the FPGA. I am wondering if I will need any additional signal conditioning before feeding siginal to AD8302?

2) Reading through other posts, it seems AD8302 becomes less accurate when the phases of the two signal are close. Can someone explain what range is considered "close"? What's the error range in this case? What the error when the phases of the two signals are, say, 90 degree apart?

Thanks in advance!

Parents
  • Dear jdobler,

    It was 0.4V Vpp. I tried again this morning: powering up the board without any input. I am still getting 3.7V VMAG output on the scope (DC coupling), 5.2V VPHS measured 5.2V.

    I asked the technician who changed the capacitors for me to double check the capacitors he changed. He thought it was done correctly.

    Thanks again!

Reply
  • Dear jdobler,

    It was 0.4V Vpp. I tried again this morning: powering up the board without any input. I am still getting 3.7V VMAG output on the scope (DC coupling), 5.2V VPHS measured 5.2V.

    I asked the technician who changed the capacitors for me to double check the capacitors he changed. He thought it was done correctly.

    Thanks again!

Children
No Data