Post Go back to editing

AD8370 Dual Supply - Serial Interface Levels

I'm using the AD8370 in a design.  I'm using it as shown in figure 51 of the data sheet, DC coupled with +/- 2.5V supplies. I can't get an output from the VGA even though the power, serial control signals and input look good.  The only thing I'm wondering about is the levels on the serial control signals.  My control signals toggle between 0V and +2.5V.  I'm wondering if they should toggle between -2.5V for a low and +2.5V for a high.  Any ideas?

Thanks,

Parents
  • Thanks for the info.  My control signals are driven by a level shifter.  I was able to AC couple the control signals and drive the level shifter from +5V.  This resulted in a +/-2.5V swing on the control signals and I was able to program the device.  It's a kludge but it works.  I wish this was more explicitly defined in the data sheet but I should known better.

    Thanks,

    -Bill

Reply
  • Thanks for the info.  My control signals are driven by a level shifter.  I was able to AC couple the control signals and drive the level shifter from +5V.  This resulted in a +/-2.5V swing on the control signals and I was able to program the device.  It's a kludge but it works.  I wish this was more explicitly defined in the data sheet but I should known better.

    Thanks,

    -Bill

Children