Post Go back to editing

HMC7282B evaluation board

Hi,

Is there any evaluation boards available for HMC7282B? Can  I have the following information and clarification?

1. Application notes for HMC7282B evaluation kit.

2. The max data rate value is denoted as 32Gbps as minimum parameter on page 2. In a scenario when the data rate is 25Gbps, can the HMC7282B eva kit amplify a 500mVpp input to 7-7.5Vpp output?

3. On page 1, it is mentioned that HMC7282B has 50ohm matced AC coupled RF inputs and outputs. However, on page 7 it mentioneds, a DC-coupled input voltage is required. Which one is correct-AC or DC coupled inputs?