Is it possible to bias this part with +3.3v? Is there a similar part that will run on +3.3v?
Thanks,
Tim
HMC858
Recommended for New Designs
The HMC858LC4B is a 2:1 Selector designed to sup-port data transmission rates of up to 14 Gbps, and selector port operation of up to 14 GHz. The selector...
Datasheet
HMC858 on Analog.com
Is it possible to bias this part with +3.3v? Is there a similar part that will run on +3.3v?
Thanks,
Tim
Copied from previous email conversion:
Is the customer looking for differential input/output I/O’s? If yes, HMC858 is the recommended part.
If his application can use single-ended I/O, HMC748LC3C might be lower cost and default for +3.3V for his 7.6Gbps should be sufficient.
http://www.hittite.com/products/view.html/view/HMC748LC3C
Yes, he can design his board to reference all GND pin to +3.3V and ground the Vee terminal and bias up and set the common mode as 3.3V CML for the I/O’s.