Post Go back to editing

Wide band mixer and 90deg phase shifter available?

HI, 

Looking for:

a) A wide band mixer that has at least the following characteristics: 

  1. Input signal frequency range: DC-5.5 GHz
  2. LO: 80 MHz
  3. Output Frequency range: 200-5.5 GHz

  The mixer should support the input and output frequency ranges within the same HW (I assume that there might be some degradation in low frequencies


 

b)  90 degrees phase shift device with the following properties:

  1. Very small and low power
  2. Frequency range: DC-5.5 GHz (or as close to it as possible)

   This is for the image rejection mixer implementation.

 

Thanks

Freddy

Parents
  • Hi FreddyS,

    b) Our phase shifter devices do not cover closetoDC-5.5 GHz. And they are also not intended for your purpose.

    What you need is a 90 degree coupler, but it may not be possible to find one with such multi-octave bandwidth.

    You can try to divide your whole band into sub bands, which will also introduce extra complexity.

    Best,

    Kagan

Reply
  • Hi FreddyS,

    b) Our phase shifter devices do not cover closetoDC-5.5 GHz. And they are also not intended for your purpose.

    What you need is a 90 degree coupler, but it may not be possible to find one with such multi-octave bandwidth.

    You can try to divide your whole band into sub bands, which will also introduce extra complexity.

    Best,

    Kagan

Children
No Data