Post Go back to editing

AD8339 eval soft for win 7

Hi

The software of AD8339-EVALZ is for Win XP.

Could you tell us how to use on win 7 64bit?

and How to get the exe and MSI files as described in DS RevA 29/36? "Using the SPI Port"

Regards

moto

Parents
  • Hi,

    The software for the AD8339-EVALZ consists of two files and is on the disc that comes with the eval board. One of the files is a .exe.

    When I last tested one of these boards I just double-clicked the .exe and my WIN7 64B operating system adapted the XP-created file so that it performed normally. There is a small-format USB port on the board so just use the type A to type B cable included in the box to make the connection. The program will open as shown in the data sheet.

    Best regards,

    js

Reply
  • Hi,

    The software for the AD8339-EVALZ consists of two files and is on the disc that comes with the eval board. One of the files is a .exe.

    When I last tested one of these boards I just double-clicked the .exe and my WIN7 64B operating system adapted the XP-created file so that it performed normally. There is a small-format USB port on the board so just use the type A to type B cable included in the box to make the connection. The program will open as shown in the data sheet.

    Best regards,

    js

Children
No Data