KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
AD8339
Production
The AD8339 is a quad I/Q demodulator configured to be driven by a low noise preamplifier with differential outputs. It is optimized for the LNA in the...
Datasheet
AD8339 on Analog.com
Hi
The software of AD8339-EVALZ is for Win XP.
Could you tell us how to use on win 7 64bit?
and How to get the exe and MSI files as described in DS RevA 29/36? "Using the SPI Port"
Regards
moto
Hi,
The software for the AD8339-EVALZ consists of two files and is on the disc that comes with the eval board. One of the files is a .exe.
When I last tested one of these boards I just double-clicked the .exe and my WIN7 64B operating system adapted the XP-created file so that it performed normally. There is a small-format USB port on the board so just use the type A to type B cable included in the box to make the connection. The program will open as shown in the data sheet.
Best regards,
js
Hi JS
Thank you for your support.
I'll try to do this and that.
Could you show the suitable USB driver soft, if you can?
Thank you
Regards
moto
Hi Js
It was not USB driver trouble.
My system is "Visual Studio Runtime engine 2010" missing.
I download and install this program from Microsoft HP.
and then that error message never came up again.
It should describe about the necessary programs in datasheet , I think.
Thank you for your support.
Regards
moto