Hi,
- Is the absolute maximum input for INP still +10dBm if the input is driven single-endedly with INN terminated in 50 ohms?
- is the sampling transfer function in the datasheet a plot of the peak amplitude at the output vs the input frequency? with THA+ADC setup, the 3dB bandwidth of the frequency response from ADC was only abt 8GHz. Across the 18GHz, the gain dropped about 5.5dB. what could be the cause?
Thank you.