Post Go back to editing

HMC1061LC5

Hi,

  1. Is the absolute maximum input for INP still +10dBm if the input is driven single-endedly with INN terminated in 50 ohms?
  2. is the sampling transfer function in the datasheet a plot of the peak amplitude at the output vs the input frequency? with THA+ADC setup, the 3dB bandwidth of the frequency response from ADC was only abt 8GHz. Across the 18GHz, the gain dropped about 5.5dB. what could be the cause?

Thank you.

Parents Reply Children
No Data