Post Go back to editing

HMC516LC5 and HMC564LC4 tested parameters?


Hi there

Which of the HMC516LC5/HMC564LC4 electrical parameters are 100% tested in production before shipping to customers?

What are the guaranteed parameters?

Are there any parameters which are shipped based on sample units tests? Where can I find the details on these acceptance tests procedures?

Thank you

ysh

  • Hi Ysh,

    The HMC516LC5 is 100% tested in production to ensure that the following data sheet performance specifications are met:

    Gain: Tested at Vdd = +3 V, to ensure 18 dB data sheet minimum

    Noise Figure: Tested at Vdd = +3 V, to ensure 2.5 dB data sheet maximum

    Supply Current (Idd)(Vdd = +3V): Tested at Vdd = +3 V, to ensure 88 mA data sheet maximum

    Gain Variation Over Temperature: Not tested in production, but instead guaranteed by design and characterization.

    Additionally, though there is no data sheet specification for maximum DC leakage at the RF input and RF output pins, the RF input and RF output capacitors are tested for gross defects.

    The HMC564LC4 is 100% tested in production to ensure that the following data sheet performance specifications are met:

    Gain: Tested at Vdd = +3 V, to ensure 14 dB data sheet minimum

    Noise Figure: Tested at Vdd = +3 V, to ensure 2.2 dB data sheet maximum

    Supply Current (Idd)(Vdd = +3V): Tested at Vdd = +3 V, to ensure 75 mA data sheet maximum

    Gain Variation Over Temperature: Not tested in production, but instead guaranteed by design and characterization.

    Additionally, though there is no data sheet specification for maximum DC leakage at the RF input and RF output pins, the RF input and RF output capacitors are tested for gross defects.

    Let me know if you have additional questions.

    Regards,

    SMcBride

  • is there any kind of variance information on saturated power and P1dB

  • Hi charlesa,

    Which product are you interested in, the HMC516LC5 or HMC564LC4?

    Regards,

    SMcBride

  • Hi charlesa,

    For the HMC516LC5 neither Psat nor P1dB are guaranteed parameters meaning, the data sheet presents them as Typ. only, without Min or Max specifications. I apologize but, for typical parameters we do not have distribution data available.

    Regards,

    SMcBride

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.