Post Go back to editing

HMC812 Eval kit information

HI,

Please help to share the user guide or schematic information of the HMC812 Evaluation board.

part no. 123768-HMC812LC4 Evaluation Board - HMC812LC4 Evaluation PCB.

Also please help to share best suited DAC to interface with HMC812 for controlling attenuation.

Regards,

Sai

Parents
  • FormerMember
    0 FormerMember
on Sep 2, 2015 5:14 AM

Hi Sai,

Attached is the PCB layout and gerber files for the HMC812LC4 Evaluation Board. This is a simple EVB circuit, we do not have the user guide or schematic diagram. The layout follows the same application circuit as shown in the HMC812LC4 datasheet.

 

Take a look at AD5429/AD5439/AD5449 DAC. With the reference circuit below copied from the datasheet, it would drive the HMC812LC4's two control input voltages ranging from -3V to 0V.

 

Best.

Reply
  • FormerMember
    0 FormerMember
on Sep 2, 2015 5:14 AM

Hi Sai,

Attached is the PCB layout and gerber files for the HMC812LC4 Evaluation Board. This is a simple EVB circuit, we do not have the user guide or schematic diagram. The layout follows the same application circuit as shown in the HMC812LC4 datasheet.

 

Take a look at AD5429/AD5439/AD5449 DAC. With the reference circuit below copied from the datasheet, it would drive the HMC812LC4's two control input voltages ranging from -3V to 0V.

 

Best.

Children
No Data