I just selected this part for a project but noticed that it is not recommended for new designs, does anyone know what the recommended replacement part is?
I called AD UK to ask but was unable to get through to anyone.
KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
View All
November Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Ever wonder how EMC limits came to be and why they matter? Dive into the interesting bits of EMC limits and levels, then test your knowledge with EMC: The Interesting Bits Quiz.
Read the blog first: EMC Limits and Levels Explained: Well, the Interesting
View All
I just selected this part for a project but noticed that it is not recommended for new designs, does anyone know what the recommended replacement part is?
I called AD UK to ask but was unable to get through to anyone.
Hi Jim,
We don't have a particular part recommended as a direct replacement, but I can help you select another ADI part if you tell me more about the requirements of your application. For example, do you have any supply constraints? Do you need the same package type (SOT-89) or device type (HBT)? Any requirements for min/max gain, output power, linearity, etc?
Thanks,
SMcBride
Thanks, what I need is 1MHz to 1GHz bandwidth, total voltage gain of ~100 (so will need to cascade a couple of amps), and it needs to be 64 channels.
The input signals are ~ 5mV random pulses that will be fed to data acquisition boards, I have no constraints on package, supply voltage etc
Hi Jim,
Your total voltage gain of ~100 corresponds to 40 dB so, each amp in your cascade must provide 20 dB gain.
For pulses of 5 mV (I'm assuming peak) the second amp in your cascade will need to capable of Pout~=+4 dBm. The only part under RF & Microwave recommended for new designs that I see coming close to meeting this requirement is the AD8353. It's a 1 MHz - 2.7 GHz gain block, internally matched, with typical gain=+20 dB and typical OP1dB=+9.1 dBm. Here is a link to the product page:
http://www.analog.com/en/products/rf-microwave/rf-amplifiers/gain-blocks/ad8353.html
Regards,
SMcBride
Great, thanks for your help, I will look at that part.