Post Go back to editing

Inquiry for specification of time delay device

I found 'Delay Control Modulation Bandwidth' specification in HMC910 datasheet.

But, I can not understand meaning of 'Delay Control Modulation Bandwidth'

Please, explain meaning of 'Delay Control Modulation Bandwidth'.

Delay Control Modulation Bandwidth of HMC910 is 10MHz and Delay Control Modulation Bandwidth of HMC911 is 1.6GHz.

Please, explain difference between two spec.

Thanks in advance.

Parents
  • Hi Joungho,

    The delay control modulation bandwidth specify the maximum frequency at which the user is able to mix/module the RF signal. HMC911 extends the maximum modulation frequency (modulation bandwidth) of HMC910 to 1.6 GHz that is required in broadband test and measurement.

    Thanks

    Ahmet

Reply
  • Hi Joungho,

    The delay control modulation bandwidth specify the maximum frequency at which the user is able to mix/module the RF signal. HMC911 extends the maximum modulation frequency (modulation bandwidth) of HMC910 to 1.6 GHz that is required in broadband test and measurement.

    Thanks

    Ahmet

Children
No Data