HMC544A: DC blocks at ports RFC, RF1 and RF2

Hi,

I am working on a high speed data aquistion system. The low power RF signal of interest is DC coupled and therefore I was thinking of using the HMC544A as a switch. The datasheet looked promising (DC - 4GHz) until I have found the section that DC blocks are required. Using DC block capacitors is not an option. Would it be worth a try to leave out the DC blocks?

Thanks and best regards,

Gerald

  • Hi,

    thanks for your help!

    I checked with my system and the following conditions will apply:

    - DC voltage level of RF signal                --> up to 1.5V

    - Minimum frequency of operation           --> Down to 0Hz

    - Maximum RF signal power                   --> Max. 17dBm

    I hope this will help you.

    Thanks in advance for your help!

    Best regards,

    Gerald

  • 0
    •  Analog Employees 
    on Aug 2, 2018 3:20 PM over 2 years ago
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin