Post Go back to editing

PHEMT bias sequencing circuit

Thread Summary

The user inquires about the correct bias sequence for turning off HMC598 and HMC-ALH382/476 chips. The final answer confirms that the power-down sequence should be: remove RF, then drain voltage, followed by gate voltage. Kagan suggests using HMC980, HMC981, or HMC920 active bias controllers, which can work with lower Vdd values, or adding a series resistor at the Vdrain output to accommodate the 2.5V requirement of HMC-ALH382.
AI Generated Content

Hello.

I'm system engineer, so don't know well about PHEMT or HEMT chip.

I'd like to use HMC598 and HMC-ALH382, HMC-ALH476 like doubler or AMP.

These chips are required some bias sequence.

You can find PDF file about bias

//Design and Implementation of a Bias Sequencing Circuit for the HMC463LP5 Low Noise Amplifier//

that circuit is method how to make proper bais sequence.

They say VGG should be turned on than VDD.  I understood it and It did good.

But, when VGG is turned off, is it okay?

I think VDD will be turnd off after VGG. It may be problems.

But that application note notice only tuned off speed by using VDD' capacitor.

Now, I want to know correct bias sequence.

Could I ignore bias when chips are turnd off?

hmc463lp5_bias_sequence.pdf

I'm going to move this into the RF forum where someone should be able to help answer this question. I did find another article which might be useful as well.

http://www.analog.com/media/en/technical-documentation/application-notes/mmic_amplifier_biasing_procedure.pdf

Brandon

  • Thank you!

    I already check that PDF file. In my case, I use standard amplifier bias sequence and cascode distriuted amplifier bias sequence.

    But they focused only turn on time without turn off time.

    //

  • Hi,

    Generally, the biasing sequence for devices which have a gate voltage (amps, doublers) will be:

    1. Apply gate voltage.
    2. Apply drain voltage.
    3. Apply RF.

    The power down sequence should be those steps in reverse:

    1. Remove RF.
    2. Remove drain voltage.
    3. Remove gate voltage.

    Best Regards,

    David

  • HI,

    You can use HMC980, HMC981 and HMC920 active bias controllers, to implement the bias sequencing.

    Best,

    Kagan

  • Thank you,

    I'm using many chips and HMC_ALH382 is one of the chips, It needs +2.5V VDD.

    But, HMC980, HMC920  chips support minimum +3V~4V.

    Best Regards,

    JEREMY

  • Hi Jeremy,

    Yes datasheet min values are 3-4V for bias controllers. They can also work for lower Vdd values, depending on the DUT Idd requirement, the voltage drop may increase. On some applications people evaluate the bias controller and DUT configuration to see if they work with lower Vdd. I have seen some apps where 2.5Vdd is supplied thru HMC981.

    Another way is using a series resistor at the Vdrain output of HMC980/1. This method is also used by some people at the expense of power consumption, see attached for an example apps circuit to bias HMC-ALH382 with HMC981.

    Best,

    Kagan