Hello,
When using Direct Parallel Mode of HMC624A, what termination is required to CLK, SERIN, SEROUT, PUP1 and PUP2? Pull-up, Pull-down, Open, termination to GND or x ohm termination to GND?
Please give an answer within this week.
Best Regards,
HMC624A
Recommended for New Designs
The HMC624A is a 6-bit digital attenuator with a 31.5 dB attenuation control range in 0.5 dB steps.
The HMC624A offers excellent attenuation accuracy and...
Datasheet
HMC624A on Analog.com
Hello,
When using Direct Parallel Mode of HMC624A, what termination is required to CLK, SERIN, SEROUT, PUP1 and PUP2? Pull-up, Pull-down, Open, termination to GND or x ohm termination to GND?
Please give an answer within this week.
Best Regards,
I have this question too. The datasheet explicitly states the D5 to D0 pins lack pulls and must not be left floating but says nothing about the pins listed above.
It looks like someone probably responded, but their response was removed.
Can anyone at AD answer please?
When the part is used in parallel mode, we don’t prefer to leave unused pins such as SERIN/CLK floating. Instead, SERIN and CLK could be pulled down to ground so that they have a defined voltage.