What is the phase noise of HMC439 at 10Hz offset for 10 MHz pdf?

Hello,

I will use HMC439 in a 100MHz clock generator application with 10 MHz pfd comparison frequency and i need phase noise data at 10Hz offset. In the datasheet it starts at 100Hz and I see a peak near 100 Hz. How is its behaviour below 100Hz? Also can I assume 10 dB decrease in 100MHz phase noise data when using it for 10MHz operation?

Thank you,

Mustafa

Parents Reply Children
No Data