Do you have an application note that discusses how to increase the output current of the HMC920 in order to use the controller with higher power devices like the HMC7357?
Thanks
Sampie
Do you have an application note that discusses how to increase the output current of the HMC920 in order to use the controller with higher power devices like the HMC7357?
Thanks
Sampie
Hi Sampie,
You can use multiple number of HMC920s to increase the Idrain capability. HMC920 is rated up to 500 mA. HMC7357`s default bias configuration requires 1.2A, so you will need 3x HMC920s.
You can also bias HMC7357, by using HMC980, which can deliver 1.2A for HMC7357.
Attached sch shows using multiple number of bias controller to increase the drain output current capability. The bias controller used on the attached SCH is HMC980, and this circuit is tested and used by us and by our customers. Same idea can be used for HMC920.
Best,
Kagan
Hi Sampie,
You can use multiple number of HMC920s to increase the Idrain capability. HMC920 is rated up to 500 mA. HMC7357`s default bias configuration requires 1.2A, so you will need 3x HMC920s.
You can also bias HMC7357, by using HMC980, which can deliver 1.2A for HMC7357.
Attached sch shows using multiple number of bias controller to increase the drain output current capability. The bias controller used on the attached SCH is HMC980, and this circuit is tested and used by us and by our customers. Same idea can be used for HMC920.
Best,
Kagan
Hi Kagan:
I use HMC980 to BIAS HMC7357, here is the SCH ,refer to your SCH. But there is a strange phenomenon: After power on 2~3s,HMC7357 has a about 20db Gain,continues about 10s then the signal disappeared。 What‘s the most probable cause can it be? Is my SCH right? Thanks a lot。
Best,
Kaka
Hi Kaka,
When you say the signal disappears do you mean the part stops functioning entirely? How does the DC look while this is happening? Could you tell me your bias sequencing?
Also, the schematic seems reasonable but since this inquiry was asked we have developed a calculator to select discrete components. I would suggest going over your circuit with this to ensure that the values are correct.
https://wiki.analog.com/resources/eval/user-guides/active-bias-controllers/hmc980?s[]=hmc980
Thanks,
DanO